You cannot export this page, because it is not available in the current version, variant, or language.
You cannot export this page, because it is not available in the current version, variant, or language.
You are viewing an old version of this page. View the current version.
Compare with Current View Page History
« Previous Version 4 Next »
This User's Manual (Application Note) explains GStreamer and the custom plug-ins created by Renesas.
Usage examples are also included.
Sample code for using GStreamer on Renesas RZ devices are stored in github.
For most common use cases, refer to the gstreamer user's manual linked above. Below are reported other specific cases not covered in that document.
gst-launch-1.0 v4l2src device=/dev/video0 num-buffers=300 ! video/x-raw,width=1280,height=960 ! vspmfilter dmabuf-use=true ! video/x-raw,format=NV12 ! omxh264enc control-rate=2 target-bitrate=10485760 interval_intraframes=14 periodicty-idr=2 ! video/x-h264,profile=\(string\)high,level=\(string\)4.2 ! filesink location=output_xsga.264
Let create a file named test.sdp and copy the below content in the file
NOTE: The IP address is the IP4 is the IP address of the stream sender
m=video 9001 RTP/AVP 96, 9001 is the port number which needs to be matched with the sender port
v=0 i=RZ Board Demo c=IN IP4 192.168.86.57 s=ESP H264 STREAM m=video 9001 RTP/AVP 96 a=rtpmap:96 H264/90000
Save the file and launch the VLC application by clicking test.sdp file to receive the stream.
NOTE: host ip address is the ip address of PC running VLC application gst-launch-1.0 -v videotestsrc ! queue ! videoconvert ! queue ! video/x-raw, width=320, height=240 ! queue ! omxh264enc ! queue ! rtph264pay ! queue ! udpsink host= 192.168.86.36 port=9001
gst-launch-1.0 --gst-debug=3 v4l2src device=/dev/video1 ! video/x-raw, width=1280, height=720 ! videoconvert \ ! video/x-raw, format=NV12 ! omxh264enc control-rate=2 target-bitrate=10485760 interval_intraframes=14 periodicty-idr=2 use-dmabuf=false \ ! video/x-h264, profile=\(string\)high,level=\(string\)4.2 ! h264parse ! rtph264pay ! queue ! udpsink host=192.168.86.36 port=9001
gst-launch-1.0 -v filesrc location=sintel_trailer-1080p.mp4 ! decodebin ! omxh264enc ! rtph264pay ! udpsink host=192.168.86.36 port=9001
Here is a an example of how to use the GStreamer C Code API for the RZV and RZG. The demo utilizes the RZ H.264 and VSPM library.
Compared to the big brothers the RZ/G2UL does not feature a GPU nor a HW video encoder / decoder. Nevertheless gstreamer can still be used, mainly using SW plugins and the CPU and, of course, the performance is limited due to this.
Since many VLP releases now, v412-init.sh
is installed by default on the /home/root folder. It has to be run before the following commands can be given.
gst-launch-1.0 v4l2src device=/dev/video0 ! video/x-raw,format=ARGB,width=1280,height=960 ! vspmfilter outbuf-alloc=true ! waylandsink
gst-launch-1.0 v4l2src device=/dev/video0 ! video/x-raw,format=ARGB,width=1280,height=960 ! vspmfilter outbuf-alloc=true ! video/x-raw, format=BGRA, width=640, height=480 ! waylandsink
As mentioned there's no HW video decoder, so SW decoding gstreamer plugins have to be used. Low resolution videos are normally played ok, medium / high resolution may be challenging.
gst-launch-1.0 filesrc location=./[VP8 encoded file].webm ! matroskademux ! avdec_vp8 ! videoconvert ! waylandsink
gst-launch-1.0 filesrc location=./[VP9 encoded file].webm ! matroskademux ! avdec_vp9 ! videoconvert ! waylandsink
gst-launch-1.0 filesrc location=./[H.264 encoded file].mp4 ! qtdemux ! h264parse ! avdec_h264 ! videoconvert ! waylandsink
gst-launch-1.0 filesrc location=./[H.264 encoded file].mp4 ! qtdemux ! h264parse ! avdec_h264 ! videoscale ! videoconvert ! video/x-raw, width=640, height=480 ! waylandsink