Versions Compared

Key

  • This line was added.
  • This line was removed.
  • Formatting was changed.

...

Some RX MCU peripherals use only fixed interrupt vectors, while some others also use software configurable interrupt vectors.
The software configurable interrupt vectors can configure which interrupt is enable by user depending on the application.

Image ModifiedImage Modified

It depends on which driver is used if you use a software configurable interrupt.

...

This is an example for GTCIU2 setting in GPT:Image Removed

Image Added

 
To resolve this error, you must configure additional interrupt settings in the "Interrupt tab".
As shown in the figure below, you need to select the interrupt from the corresponding interrupt vector group, INTA or INTB.

Image Modified

Please also refer to the "User's Manual: Hardware" of each product to determine whether the interrupt belongs to INTA or INTB.This information shows as table

The table for this information is shown in the section as follows in Users following section of the "User's Manual: Hardware":

  • Software Configurable Interrupt A Source Select Register n
  • Software Configurable Interrupt B Source Select Register n 

...

Image Added

How to check the software configurable interrupt is applied

Please check the r_bsp_interrupt_config.h located in the src/smc_gen/r_config/.Image Removed

Image Added

The If the software configurable interrupt setting is not applied correctly, the vector table may be set as blankto blank if the software configurable interrupt setting fails.

Image Modified