You are viewing an old version of this page. View the current version.

Compare with Current View Page History

« Previous Version 13 Next »


Some RX MCU peripherals use only fixed interrupt vectors, while some others also use software configurable interrupt vectors.
The software configurable interrupt vectors can configure which interrupt is enable by user depending on the application.

It depends on which driver is used if you use a software configurable interrupt.

How to set the software conifugurable interrupt

This is an example for GTCIU2 setting in GPT:

 
To resolve this error, you must configure additional interrupt settings in the "Interrupt tab".
As shown in the figure below, you need to select the interrupt from the corresponding interrupt vector group, INTA or INTB.

Please also refer to the "User Manual: Hardware" of each product to determine whether the interrupt belongs to INTA or INTB.
This information shows as table in the section as follows in Users Manual:Hardware:

  • Software Configurable Interrupt A Source Select Register n
  • Software Configurable Interrupt B Source Select Register n 

How to check the software configurable interrupt is applied

Please check the r_bsp_interrupt_config.h located in the src/smc_gen/r_config/.

If the software configurable interrupt setting is not applied correctly, the vector table may be set as blank.



  • No labels