Versions Compared

Key

  • This line was added.
  • This line was removed.
  • Formatting was changed.

Overview

This page is for quick tips to help you with Flash Self-programming RL78 MCUs.  

...

RL78 Flash Self Programming Considerations

In RL78 series MCUs,

...

a special RAM area is allocated by flash self programming library.  This RAM area is called self-RAM.  User not aware of this, may see unexpected behaviors when using the RL78 series Flash Self-Programming Library to erase and program RL78 MCUs in field.  

The relevant application documentation for the RL78 series Flash Self-Programming Library includes descriptions of

...

self-RAM.  For example, the section 9.4 "Defining the Internal RAM Area" in the RL78 Family Flash Self-Programming Library Type01 Package Ver.4.00 Release Note provides detailed information about

...

self-RAM allocation and its usage.

...

 

RL78 Family Flash Self-Programming Library Type01 Package Ver.4.00