You are viewing an old version of this page. View the current version.

Compare with Current View Page History

« Previous Version 2 Current »

RL78 Flash Self Programming Considerations

In RL78 series MCUs, a special RAM area is allocated by flash self programming library.  This RAM area is called self-RAM.  User not aware of this, may see unexpected behaviors when using the RL78 series Flash Self-Programming Library to erase and program RL78 MCUs in field.  

The relevant application documentation for the RL78 series Flash Self-Programming Library includes descriptions of self-RAM.  For example, the section 9.4 "Defining the Internal RAM Area" in the RL78 Family Flash Self-Programming Library Type01 Package Ver.4.00 Release Note provides detailed information about self-RAM allocation and its usage. 

RL78 Family Flash Self-Programming Library Type01 Package Ver.4.00

  • No labels