Versions Compared

Key

  • This line was added.
  • This line was removed.
  • Formatting was changed.
  HTML<font size=6><B>RA Series

RA Series 32-bit

MCUs</B></font>

MCUsImage Added

Introduction

Image Removed

This page is for the Renesas RA family of MCUs. The main goal is to make the information about RA MCUs friendly, easy to access for embedded developers.

The links below can be used to get familiar with Renesas RA MCUs. 

Getting Started with RA

Here are the resources for RA MCUs on Renesas GitHub site.

  • Flexible Software Package (FPSFSP)
  • Example Projects (EPs)
  • Application Project (APs

Other resources on Renesas Website.  Links below are pre-configured searches.  You can modify them as needed.  

First RA Project

 Steps below are for creating a simple Blinky project with Renesas supported tools.  e2studio is the Renesas supported IDE. You can also use EWARM and Keil IDEs.  Supported toolchains are Arm GNU Toolchain, LLVM Embedded Toolchain for Arm, IAR Compiler, and Arm Compiler.  

  • Download the latest FSP platform installer from here for e2studio for Windows.  It includes Arm GNU and LLVM toolchains.  

Official Software and Documentation

These are the currently supported Software packages for the RZA1 and RZA2M. The

Renesas Supported Development Environments

  • Renesas e2studio
  • RZA1 Smart Configurator
    • NOTE: The RZA1 is not supported on the Smart Configurator found in the Renesas e2studio IDE.
    • This Smart Conjugator is a standalone application
    • Hardware Pin Configuration is supported
    • Code Generation not supported

RZA GUI Platforms

RZA Bootloaders

Below are links to Source code for the RZ/A bootloaders and firmware update. These are reference code that was designed for the Renesas RZ/A EVKs. Included below are links to porting documentation.

RZA1

  • RZ/A1 Bootloader
    • RZ/A1H Group Example of Booting from Serial Flash Memory doc and Source Code
    • RZ/A1LU QSPI Flash Boot Loader doc and Source Code
    • RZ/A1LU Group Example of Booting from Serial Flash Memory doc and Source Code
  • RZA firmware update
    • The RZA1 does not have Firmware Update reference code.
    • Refer to the RZA2M Firmware Update for Serial Flash Driver to port to the RZA1.

RZA2M

Porting Guides

RZ/A1

  • RZ/A1 Azure Porting Guide gear Wiki

Articles and Whitepapers

Topics

FAQ

  • Hardware Related
  • Common RZA IDE issues
  •   3rd party IDEs and toolchains are supported by respective partner companies.  

    Each FSP version and supported tools are available from the Releases page.  Bundled platform installers are available at the bottom of each FSP version under Assets section.   

    Boards

    Official Renesas RA series boards are available here.  Each board has its landing page and most have the following information. 

    • Board Quick Start Guide
    • Board User's Manual
    • Board Design Package 

    Your First RA Project

    This is your first RA project, designed to blink the LEDs on the EK-RA8D1 board.  It serves as an introduction to e2studio, the RA project creator, and the FSP Configurator.  The process outlined applies to all official Renesas RA series boards.  Additionally, this project provides a simple way to verify that your development environment is set up correctly and that all necessary tools are functioning properly.

    Your First RA Project

    Tips and Tricks

    RA Tips and Tricks page page contains many useful information and how to notes on everything RA.  We update the page regularly so come and check it often.   

    Known Issues and Workarounds

    RA Issues page lists known bugs and possible workarounds for HW, SW, and tools.  

    RA Specific Topics

    This is to discuss specific topics for RA.  Each topic discussed here can be detailed and lengthy.  Therefore, RA Specific Topics page serves as a table of contents with a short description of the topics followed by a dedicated page for that subject.   

    RZA FreeRTOS




    Table of Contents