Image Modified
HTML |
---|
<font size=6><B>RZ/A Series 32/64-bit MPUs</B></font>
<br><font size=+1>This page is for the Renesas RZ/A family of embedded SoCs. The main goal is to make the information about RZ/A SoCs friendly, easy to access for embedded developers.</font>
<p align=right><B>RZ = Renesas Zenith</B></p>
<! To make a ToC move/scroll with the page >
<style> .toc-macro {position: static !important;} </style>
<! Make the ToC in-line (not float on the right) >
<style> .toc-macro {float: none !important;} </style>
<! To make a ToC wider >
<style> .toc-macro {width: 600px !important;} </style>
<! Transparent background (no color) >
<style> .toc-macro {background: transparent !important;} </style>
<! To make a ToC Font Size bigger. Default font-size: 15px. Default line-height: 1.6 >
<style> .toc-item-body {font-size: 18px !important;} </style> |
Image Added
Online Resources
...
The links below can be used to get familiar with Renesas RZ/A SoC
Ordering Part Numbers
Boards
- Here is the list of available Renesas Evaluation Boards (bottom of page).
- The board pages below contain instructions for downloading and building the BSP as well as other useful information about the boards.
RZ/A3 Series Evaluation Boards
...
...
RZ/A3UL Evaluation board Image Modifiedby Renesas
|
RZ/A2M Series Evaluation Boards
...
...
RZ/A1 Series Evaluation Boards
...
Section |
---|
Column |
---|
| RZ/A1UL GR-LYCHEE
Image Modified by Renesas MBED |
Column |
---|
| RZ/A1H GR-PEACH Image Modified by Renesas MBED |
|
Official Software and Documentation
These are the currently supported Software packages for the RZA1 and RZA2M. The
Renesas Supported Development Environments
- Renesas e2studio
- RZA1 Smart Configurator
- NOTE: The RZA1 is not supported on the Smart Configurator found in the Renesas e2studio IDE.
- This Smart Conjugator is a standalone application
- Hardware Pin Configuration is supported
- Code Generation not supported
RZA GUI Platforms
- Microsoft Azure GUIX demos
- TES Guiliani
- Crank contact Crank for RZA demos
- MicroEJ contact MicroEJ for RZA Java demos
- Tara Embedded Wizard contact Tara for RZA demos
RZA Bootloaders
Below are links to Source code for the RZ/A bootloaders and firmware update. These are reference code that was designed for the Renesas RZ/A EVKs. Included below are links to porting documentation.
RZA1
- RZ/A1 Bootloader
- RZA firmware update
- The RZA1 does not have Firmware Update reference code.
- Refer to the RZA2M Firmware Update for Serial Flash Driver to port to the RZA1.
RZA2M
- RZ/A2M Group Example of booting from OctaFlash™ using SPI multi I/O bus controller
- RZA2M Firmware update ( rza2m_fw_update_sample_freertos_gcc.zip )
Porting Guides
RZ/A1
- RZ/A1 Azure Porting Guide Wiki
Articles and Whitepapers
Topics
FAQ
...
...
...