If you encounter any issues after the upgrade, please open a support request TICKET.🙌
Image RemovedThis page is for the Renesas RA family of MCUs. The main goal is to make the information about RA MCUs friendly, easy to access for embedded developers.
The links below can be used to get familiar with Renesas RA MCUs.
Here are the resources for RA MCUs on Renesas GitHub site.
Other resources on Renesas Website. Links below are pre-configured searches. You can modify them as needed.
Steps below are for creating a simple Blinky project with Renesas supported tools. e2studio is the Renesas supported IDE. You can also use EWARM and Keil IDEs. Supported toolchains are Arm GNU Toolchain, LLVM Embedded Toolchain for Arm, IAR Compiler, and Arm Compiler.
These are the currently supported Software packages for the RZA1 and RZA2M. The
Below are links to Source code for the RZ/A bootloaders and firmware update. These are reference code that was designed for the Renesas RZ/A EVKs. Included below are links to porting documentation.
RZA1
RZA2M
RZ/A1
3rd party IDEs and toolchains are supported by respective partner companies.
Each FSP version and supported tools are available from the Releases page. Bundled platform installers are available at the bottom of each FSP version under Assets section.
Official Renesas RA series boards are available here. Each board has its landing page and most have the following information.
This is your first RA project, designed to blink the LEDs on the EK-RA8D1 board. It serves as an introduction to e2studio, the RA project creator, and the FSP Configurator. The process outlined applies to all official Renesas RA series boards. Additionally, this project provides a simple way to verify that your development environment is set up correctly and that all necessary tools are functioning properly.
RA Tips and Tricks page page contains many useful information and how to notes on everything RA. We update the page regularly so come and check it often.
RA Issues page lists known bugs and possible workarounds for HW, SW, and tools.
This is to discuss specific topics for RA. Each topic discussed here can be detailed and lengthy. Therefore, RA Specific Topics page serves as a table of contents with a short description of the topics followed by a dedicated page for that subject.
RZA FreeRTOSTable of Contents |
---|