General Information

  • Free, open-source based library of pre-trained AI applications available on github.
  • ⭐Source Code: https://github.com/Ignitarium-Renesas/RZV2L_AiLibrary
  • This Library has API functions for leveraging AI applications that will run on Renesas RZ/V2L Board. Currently this library has following sample applications:
    • Human Head Counter
    • Line crossing object Counter
    • Elderly people fall detection (Work in progress)
    • Safety helmet and vest detection
    • Human age and gender detection (Work in progress)
    • Face recognition and spoof detection (Work in progress

Pre-Trained AI Article

Addition Notes

The Pre-trained models include pre-compiled applications as well as AI Models translated to run on the DRP-AI hardware. These files are located in the "exe" folder for each Pre-trained Application. These precompiled application are compiled for the Renesas RZV2L EVK using the Coral MIPI Camera. This folder can be simple copied to the board using SCP recursive command. NOTE : Some Pre-trained Applicatino

Support USB Camera

By default the Pretrained Applications are compiled to use the MIPI camera. The Pre-trained applications can be modified to use USB camera. This modification is only relevant to applications that support video.

  1. Open the application folder src folder. For example 01_Head_count/Head_count_cam/src
  2. Open the define.h header file.
  3. Find the following line. Comment out the macro that defines INPUT_CORAL.
/* Coral Camera support */
#define INPUT_CORAL

Sample Videos

NOTE: Memory Usage includes the Image Input, Inference Output, Inference Weights and Inference Parameters. Applications that use multiple AI Models are run sequentially


Head Count Application


Model : YoloV3
Memory Usage: 235MB
Inference Input Shape : 416,416,3
Inference Time: 348ms



Head Count


Line Crossing Object Counting


Model : TinyYoloV2
Memory Usage: 52MB
Inference Input Shape : 416,416,3
Inference Time:



Line Count


Fall Detection


Model : Tiny Yolov2
Memory Usage: 52MB
Inference Input Shape : 256, 192, 3
Inference Time: 59ms
Model : HRNET
Memory Usage: 129MB
Inference Input Shape : 256, 192, 3
Inference Time: 163ms
Total Inference Time : 222ms



Fall Detection


Age and Gender Detection


Model : Custom age
Memory Usage: 24MB
Inference Input Shape : 416,416,3
Inference Time: 10ms
Model : Custom gender
Memory Usage: 87MB
Inference Input Shape : 224,224,3
Inference Time: 10ms
Model : Tiny YoloV2
Memory Usage: 52MB
Inference Input Shape : 416,416,3
Inference Time: 59ms
Total Inference Time: 79ms



Age and Gender Detection


Face Recognition, Spoofing, and Registration


Model : Resnet50
Memory Usage: 88MB
Inference Input Shape : 224,224,3
Inference Time: 96ms



Face Recognition


Animal Detection


Model : YoloV3
Memory Usage: 236MB
Inference Input Shape : 416,416,3
Inference Time: 360ms



Animal Detection


Hand Gesture Recognition


Model : Custom Pose Detector for Hand
Memory Usage: 91MB
Inference Input Shape : 256,256,3
Inference Time: 256ms



Hand Gesture Recognition


Human Gaze Recognition


Model : Resnet18
Memory Usage: 38MB
Inference Input Shape : 416,416,3
Inference Time: 33
Model : Tiny YoloV2
Memory Usage: 52MB
Inference Input Shape : 416,416,3
Inference Time: 58
Total Inference Time: 91ms



Gaze Recognition


  • No labels