- The MistyWest team has prepared a plugin which can receive any kind of video input, such as a file (filesrc), a network stream (udpsrc), or a camera device (v4l2src) and outputs a video with bounding boxes on inferred objects using the DRPAI. Later, this video can be linked to any kind of output, such as the display (autovideosink), a network stream (udpsink), or a file (filesink).
- The plugin is available publicly with a MIT License
- https://github.com/MistySOM/gstreamer1.0-drpai
Short description on how to setup a docker image and container to be used at the RZ MPU.
1. enable docker within VLP build by uncommenting the following line within the yocto configuration file (local.conf):
#MACHINE_FEATURES_append = " docker"
=>
MACHINE_FEATURES_append = " docker"
2. Setup the EVK and verify that Docker Engine is installed correctly by running the hello-world image.
docker run hello-world
3. Define docker names (as you like)
export DOCKER_HOME=/home/root/docker
export IMAGE_NAME=rzv2l
export CONTAINER_NAME=rzv2l_container
mkdir -p ${DOCKER_HOME}
4. create docker image from scratch:
cat core-image-minimal-smarc-rzv2l.tar | docker import - ${IMAGE_NAME}
5. start container (--rm removes the container after exiting docker)
docker run -it \
--name=${CONTAINER_NAME} \
--privileged \
--rm \
--volume="/home/$USER/RZV_AI_Eva_SW:${DOCKER_HOME}/RZV_AI_Eva_SW" \
--workdir=${DOCKER_HOME} \
${IMAGE_NAME} bash