You are viewing an old version of this page. View the current version.

Compare with Current View Page History

Β« Previous Version 8 Next Β»



Device Tree and Device Driver Information

This page contains helpful notes about Device Tree configurations

RZ Evaluation Board Files

  • Device Tree files for Renesas SoC and evaluation boards are under the directory arch/arm64/boot/dts/renesas/
  • Below is the list of Device Tree files used for the Renesas Evaluation boards.
  • Because the evaluation kits share common boards, and have many different test/demo configurations, there are many include files (.dtsi) for any single device tree (.dts) build. For your custom board, you might only need your Device Tree for your board (my_board.dst) and that will only #include one other file which will be the base SoC file (RZ/G2H for example will #include "r8a774e1.dtsi").
  • RZ board names that end in "-dev" are internal Renesas boards. While their Device Trees files appear in the BSP, they are not mainlined.


FileDescription
r8a774e1.dtsiRZ/G2H Device Tree containing all peripherals

 
r8a774e1-hihope-rzg2h.dtsMain board only
r8a774e1-hihope-rzg2h.dts
β”œβ”€r8a774e1.dtsi
└─hihope-rev4.dtsi
  └─hihope-common.dtsi
r8a774e1-hihope-rzg2h-ex.dtsMain board + Sub board
r8a774e1-hihope-rzg2h-ex.dts
β”œβ”€r8a774e1-hihope-rzg2h.dts
β”‚ β”œβ”€r8a774e1.dtsi
β”‚ └─hihope-rev4.dtsi
β”‚   └─hihope-common.dtsi
└─hihope-rzg2-ex.dtsi
r8a774e1-hihope-rzg2h-ex-idk-1110wr.dtsMain board + Sub board + LVDS panel
r8a774e1-hihope-rzg2h-ex-idk-1110wr.dts
β”œβ”€r8a774e1-hihope-rzg2h-ex.dts
β”‚ β”œβ”€r8a774e1-hihope-rzg2h.dts
β”‚ β”‚  β”œβ”€r8a774e1.dtsi
β”‚ β”‚  └─hihope-rev4.dtsi
β”‚ β”‚    └─hihope-common.dtsi
β”‚ └─hihope-rzg2-ex.dtsi
β”œβ”€hihope-rzg2-ex-lvds.dtsi
└─rzg2-advantech-idk-1110wr-panel.dtsi
r8a774e1-hihope-rzg2h-ex-mipi-2.1.dtsMain board + Sub board + MIPI-CSI2 cameras
r8a774e1-hihope-rzg2h-ex-mipi-2.1.dts
β”œβ”€r8a774e1-hihope-rzg2h-ex.dts
β”‚ β”œβ”€r8a774e1-hihope-rzg2h.dts
β”‚ β”‚ β”œβ”€r8a774e1.dtsi
β”‚ β”‚ └─hihope-rev4.dtsi
β”‚ β”‚   └─hihope-common.dtsi
β”‚ └─hihope-rzg2-ex.dtsi
└─hihope-rzg2-ex-aistarvision-mipi-adapter-2.1.dtsi
  └─aistarvision-mipi-adapter-2.1.dtsi
r8a774e1-hihope-rzg2h-ex-mipi-2.4.dtsMain board + Sub board + MIPI-CSI2 cameras
r8a774e1-hihope-rzg2h-ex-mipi-2.4.dts
β”œβ”€r8a774e1-hihope-rzg2h-ex.dts
β”‚ β”œβ”€r8a774e1-hihope-rzg2h.dts
β”‚ β”‚ β”œβ”€r8a774e1.dtsi
β”‚ β”‚ └─hihope-rev4.dtsi
β”‚ β”‚   └─hihope-common.dtsi
β”‚ └─hihope-rzg2-ex.dtsi
└─hihope-rzg2-ex-aistarvision-mipi-adapter-2.4.dtsi
  └─aistarvision-mipi-adapter-2.4.dtsi
FileDescription
r8a774b1.dtsiRZ/G2N Device Tree containing all peripherals


r8a774b1-hihope-rzg2n.dtsMain board only
r8a774b1-hihope-rzg2n-ex.dtsMain board + Sub board
r8a774b1-hihope-rzg2n-ex-idk-1110wr.dtsMain board + Sub board + LVDS panel
r8a774b1-hihope-rzg2n-ex-mipi-2.1.dtsMain board + Sub board + MIPI/CSI2 cameras
r8a774b1-hihope-rzg2n-ex-mipi-2.4.dtsMain board + Sub board + MIPI/CSI2 cameras
r8a774b1-hihope-rzg2n-rev2.dts
r8a774b1-hihope-rzg2n-rev2-ex.dts
r8a774b1-hihope-rzg2n-rev2-ex-idk-1110wr.dts
rzg2-advantech-idk-1110wr-panel.dtsi
r8a774b1-hihope-rzg2n-rev2-ex-mipi-2.1.dtsMain board + Sub board + MIPI/CSI2 cameras
r8a774b1-hihope-rzg2n-rev2-ex-mipi-2.4.dtsMain board + Sub board + MIPI/CSI2 cameras
FileDescription
r8a774a1.dtsiRZ/G2M Device Tree containing all peripherals


r8a774a1-hihope-rzg2m.dtsMain board only
r8a774a1-hihope-rzg2m-ex.dtsMain board + Sub board
r8a774a1-hihope-rzg2m-ex-idk-1110wr.dtsMain board + Sub board + LVDS panel
rzg2-advantech-idk-1110wr-panel.dtsiMain board + Sub board + LVDS panel
r8a774a1-hihope-rzg2m-ex-mipi-2.1.dts
r8a774a1-hihope-rzg2m-ex-mipi-2.4.dts
r8a774a1-hihope-rzg2m-rev2.dts
r8a774a1-hihope-rzg2m-rev2-ex.dts
r8a774a1-hihope-rzg2m-rev2-ex-idk-1110wr.dts
r8a774a1-hihope-rzg2m-rev2-ex-mipi-2.1.dtsMain board + Sub board + MIPI/CSI2 cameras
r8a774a1-hihope-rzg2m-rev2-ex-mipi-2.4.dtsMain board + Sub board + MIPI/CSI2 cameras
r8a774a3.dtsi
r8a774a3-hihope-rzg2m.dts
r8a774a3-hihope-rzg2m-ex.dts
r8a774a3-hihope-rzg2m-ex-idk-1110wr.dts
rzg2-advantech-idk-1110wr-panel.dtsi
r8a774a3-hihope-rzg2m-ex-mipi-2.1.dtsMain board + Sub board + MIPI/CSI2 cameras
r8a774a3-hihope-rzg2m-ex-mipi-2.4.dtsMain board + Sub board + MIPI/CSI2 cameras
FileDescription
r8a774c0.dtsiRZ/G2E Device Tree containing all peripherals


r8a774c0-cat874.dtsMain board only
r8a774c0-cat874.dts
β”œβ”€r8a774c0.dtsi
└─cat874-common.dtsi
r8a774c0-ek874.dtsMain board + Sub board
r8a774c0-ek874.dts
β”œβ”€r8a774c0-cat874.dts
β”‚ β”œβ”€r8a774c0.dtsi
β”‚ └─cat874-common.dtsi
└─cat875.dtsi
r8a774c0-ek874-idk-2121wr.dtsMain board + Sub board + LVDS panel
r8a774c0-ek874-mipi-2.1.dtsMain board + Sub board + MIPI/CSI2 cameras
r8a774c0-ek874-mipi-2.4.dtsMain board + Sub board + MIPI/CSI2 cameras
r8a774c0-cat874-revc.dtsMain board only (older Rev C board)
r8a774c0-ek874-revc.dtsMain board + Sub board (older Rev C board)
r8a774c0-ek874-revc-idk-2121wr.dtsMain board + Sub board + LVDS panel (older Rev C board)
r8a774c0-ek874-revc-mipi-2.1.dtsMain board + Sub board + MIPI/CSI2 cameras (older Rev C board)
r8a774c0-ek874-revc-mipi-2.4.dtsMain board + Sub board + MIPI/CSI2 cameras (older Rev C board)
r8a774c0-es10-cat874.dtsMain board only (older Rev 1.0 board)
r8a774c0-es10-ek874.dtsMain board + Sub board (older Rev 1.0 board)
r8a774c0-es10-ek874-idk-2121wr.dtsMain board + Sub board + LVDS panel (older Rev 1.0 board)
r8a774c0-es10-ek874-mipi-2.1.dtsMain board + Sub board + MIPI/CSI2 cameras (older Rev 1.0 board)
r8a774c0-es10-ek874-mipi-2.4.dtsMain board + Sub board + MIPI/CSI2 cameras (older Rev 1.0 board
FileDescription
r9a07g044.dtsiRZ/G2L family SoC common parts
r9a07g044l.dtsiSpecific to RZ/G2L (R9A07G044L) SoC
r9a07g044l1.dtsiSpecific to RZ/G2L (R9A07G044L single cortex A55) SoC
r9a07g044l2.dtsiSpecific to RZ/G2L (R9A07G044L dual cortex A55) SoC


r9a07g044l2-smarc.dtsTop level Device Tree

Included files:

r9a07g044l2-smarc.dts
β”œβ”€r9a07g044l2.dtsi
β”‚ └─r9a07g044.dtsi
β”œβ”€rzg2l-smarc-som.dtsi
β”œβ”€rzg2l-smarc-pinfunction.dtsi
β”œβ”€rz-smarc-common.dtsi
└─rzg2l-smarc.dtsi
FileDescription
r9a07g044c1.dtsiRZ/G2LC Device Tree containing all peripherals
r9a07g044c2.dtsiRZ/G2LC Device Tree containing all peripherals


r9a07g044c2-smarc.dtsTop level Device Tree

Included files:

r9a07g044c2-smarc.dts
β”œβ”€r9a07g044c2.dtsi
β”‚ └─r9a07g044.dtsi
└─rzg2lc-smarc.dtsi
  β”œβ”€rzg2lc-smarc-som.dtsi
  β”œβ”€rzg2lc-smarc-pinfunction.dtsi
  └─rz-smarc-common.dtsi
FileDescription
r9a07g043.dtsiRZ/G2UL Device Tree containing all peripherals


r9a07g043u11-smarc.dtsTop level Device Tree

Included files:

r9a07g043u11-smarc.dts
β”œβ”€r9a07g043.dtsi
└─rzg2ul-smarc.dtsi
  β”œβ”€rzg2ul-smarc-som.dtsi
  β”œβ”€rzg2ul-smarc-pinfunction.dtsi
  └─rz-smarc-common.dtsi
FileDescription
r9a07g054.dtsiRZ/V2L Device Tree containing all peripherals. Use for your board.
r9a07g054l1.dtsiSets the compatible strings. Use for your board.


r9a07g054l2-smac.dtsTop level Device Tree

Defines Memory areas including video Codec, DRP-AI, Simple ISP, V4L image buf
Included files:

r9a07g054l2-smarc.dts
β”œβ”€r9a07g054l2.dtsi
β”‚ └─r9a07g054.dtsi
β”œβ”€rzg2l-smarc-som.dtsi
β”œβ”€rzg2l-smarc-pinfunction.dtsi
β”œβ”€rz-smarc-common.dtsi
└─rzg2l-smarc.dtsi
If you to see a list of which peripheral nodes are set in each file, you can use this "dts_parser" tool below. For example, you want to find all the the .dtsi files that configure the i2c channels because you are looking for examples.



Device Tree Syntax

Print a Compiled DTB Output File

  • When compiling a .dts file into a binary .dtb file, many include files might be combined.
  • Some include files might contain nodes overwrite other nodes.
  • You might not know what the final Device Tree looks like after all the includes and nodes overwrites.
  • You can install the device-tree-compiler package to show the contents of a .dtb file
$ sudo apt-get install device-tree-compiler
  • Below is an example command to print a .dtb file
$ dtc -I dtb -O dts -o - r8a774a3-hihope-rzg2m-ex.dtb

Top Level (root node)

Compatible for the SoC

  • The .dtsi file for each SoC will have a "compatible" string to specify that SoC it is. If you decide to make your own top level compatible, make sure you include the original SoC string. The reason is that some drivers (the VSP driver for example) look for that SoC string to know what SoC they are running on. If it is missing, it will not load or run correctly.

Here is a correct example of a .dts file for a RZ/G2L board. Notice how "renesas,r9a07g044" is at the end of the line.

/ {
	model = "My Really Cool RZ/G2L Board";
	compatible = "my-rzg2l-board" , "renesas,r9a07g044";

	chosen {
		bootargs = "ignore_loglevel rw root=/dev/mmc0blk1";
		stdout-path = "serial0:115200n8";
	};

};

Clocks and Resets (CPG)

  • System clocks, PLL setup, Dividers, Individual Peripheral Reset etc...
  • CPG = Clock Pulse Generator

Linux Drivers

  • RZ/G2H, G2M, G2N, G2E:
  • RZ/G2L, G2LC, G2UL, V2L:
    • drivers/clk/renesas/*
    • CONFIG_CLK_RENESAS=y
    • (drivers for individual devices are auto selected by Kconfig)

Notes

  • You generally do not have to do anything with these nodes or drivers. They are just listed here for reference.

Pin Control (pin mux)

Linux Drivers

  • RZ/G2H, G2M, G2N, G2E:
    • drivers/pinctrl/renesas/core.c, pinctrl.c, pfc-xxxx.c, etc... (refer to the Makefile)
    • CONFIG_PINCTRL_RENESAS=y
    • Documentation/devicetree/bindings/pinctrl/renesas,pcf.yaml
  • RZ/G2L, G2LC, G2UL, V2L:
    • drivers/pinctrl/renesas/pinctrl-rzg2l.c
    • CONFIG_PINCTRL_RZG2L=y
    • Documentation/devicetree/bindings/pinctrl/renesas,rzg2l-pinctrl.yaml

Notes

  • Helpful Debug Messages: Sometimes it is helpful to see how the pins are being configured on boot up. By putting #define DEBUG at the top of the driver file (pinctrl.c or pinctrl-rzg2.c) will make it print out how each pins is being configured.

Device Tree Examples

  • (see device tree for evaluation board)
  • Use any GPIO as wake-up source, e.g. P37.2:
    gpio_keys {
        compatible = "gpio-keys";
        #address-cells = <1>;
        #size-cells = <0>;
        autorepeat;

        P37_2 {
            label = "GPIO Key WAKEUP";
            linux,code = <143>;
            wakeup-source;
            interrupt-parent = <&pinctrl>;
            interrupts = <RZG2L_GPIO(37, 2) IRQ_TYPE_EDGE_FALLING>;
            debounce-interval = <50>;
        };
    };

IRQ0-7

Linux Drivers

  • RZ/G2H, G2M, G2N, G2E:
    • CONFIG_xxx=y
  • RZ/G2L, G2LC, G2UL, V2L:
    • drivers/irqchip/irq-renesas-rzg2l.c
    • CONFIG_RENESAS_RZG2L_IRQC=y
    • Added after 'rz-5.10-cip13'

Notes

Device Tree Examples

  • Use NMI as wake-up source:
   gpio_keys {
       compatible = "gpio-keys";
       #address-cells = <1>;
       #size-cells = <0>;
       autorepeat;

       NMI {
           label = "NMI Key WAKEUP";
           linux,code = <143>;
           wakeup-source;
           interrupt-parent = <&intc_ex>;
           interrupts = <8 IRQ_TYPE_EDGE_FALLING>;
           debounce-interval = <50>;
       };
   };

&intc_ex {
    status = "okay";
};

IRQs can be used as well:

   gpio_keys {
       compatible = "gpio-keys";
       #address-cells = <1>;
       #size-cells = <0>;
       autorepeat;
       pinctrl-0 = <&user_key_pin>;

       IRQ_7 {
           label = "IRQ_7 Key WAKEUP";
           linux,code = <143>;
           wakeup-source;
           interrupt-parent = <&intc_ex>;
           interrupts = <7 IRQ_TYPE_EDGE_FALLING>;
           debounce-interval = <50>;
       };
   };

&intc_ex {
    status = "okay";
};

&pinctrl{
	user_key_pin: user_key {
		pinmux = <RZG2L_PORT_PINMUX(3, 1, 1)>;	/* IRQ7 */
	};
}; 

Display

Linux Drivers

  • Common:
    • drivers/gpu/drm/rcar-du/*
      • CONFIG_DRM_RCAR_DU=y
    • drivers/media/platform/vsp1/*
      • CONFIG_VIDEO_RENESAS_VSP1=y
  • RZ/G2H, G2M, G2N, G2E:
    • CONFIG_DRM_RCAR_LVDS=y
  • RZ/G2L, G2LC, G2UL, V2L:
    • drivers/gpu/drm/rcar-du/rzg2l_mipi_dsi.h
    • drivers/gpu/drm/rcar-du/rzg2l_mipi_dsi.c
    • drivers/gpu/drm/rcar-du/rzg2l_mipi_dsi_regs.h

Notes

  • Ports Node When defining ports { }, you must set #address-cells = <1>; and #size-cells = <0>;. For more information, see the documentation in the kernel source: Documentation/devicetree/bindings/media/video-interfaces.txt
  • Resolution and Clock Definitions: An LCD Panel will have it's own separate driver. That driver will define the clock rate and resolution. The Renesas LCD driver will then get that information in order to set up the LCD controller (DU) output.
  • MIPI DSI Overview: Here is a good article explaining the MIPI DSI interface, packets and commands. https://circuitcellar.com/resources/quickbits/mipi-display-serial-interface
  • MIPI DCS Commands: Many (most) MIPI DSI Panels require setup command (DCS) to be set over MIPI DSI to configure the panel's controller before pixel data can be sent. This is why there is usually a separate driver for each LCD since these commands are specific to each LCD panel.
  • Simple-Panel Driver: If your panel requires no special setup (no MIPI DSI DCS commands) or your system is configuring your LCD manually over I2C, or you are using a parallel RGB panel that typically requires no setup, you can use the kernel's "simple-panel" driver. The main reason is that you need to tell the kernel about the resolution and pixel timing is of your panel, but that information is not described in a Device Tree, it must come from a source code driver file. The panel-simple driver is there as a way to do that by simply adding in a new entry for your custom panel. Note that you will be required to edit the driver file (drivers/gpu/drm/panel/panel-simple.c) to add your specific panel resolution and timing that you want. See kernel documentation Documentation/devicetree/bindings/panel/simple-panel.txt.
  • Parallel RGB LCD: Since a parallel LCD does not need any special setup, you can use simple-panel driver in the kernel.
  • Check Display Settings: You can use the command modetest -M rcar-du -c to check the status of your display driver. It will also show you the supported resolutions of your display (in the case that you are using an HDMI interface where it will read what is supported by the HDMI panel).


  • Check VBLANK Timings: You can use the command vbltest -M rcar-du to check the VBLANK timings. If your result is always around 60Hz, your panel is set correctly.




Device Tree Examples:

  • RZ/G2L: MIPI-CSI to HDMI Bridge: See device tree for evaluation board.
  • Ilitek ILI9881c panel controller
  • 2-lane MIPI interface
  • 800x1280 Portrait Panel
  • Please remember "reg = <0>;" in panel@0
&du {
	status = "okay";
};

&dsi0 {
	status = "okay";
	#address-cells = <1>;
	#size-cells = <0>;
​
	ports {
			#address-cells = <1>;
			#size-cells = <0>;
​
			port@1 {
					dsi0_out: endpoint {
							remote-endpoint = <&panel_in>;
							data-lanes = <1 2>;
					};
			};
	};
​
	panel@0 {
			compatible = "ilitek,ili9881c";
			reg = <0>;
			dsi-lanes = <2>;
			enable-gpios = <&pinctrl RZG2L_GPIO(43, 0) GPIO_ACTIVE_HIGH>;
			backlight = <&backlight>;
			status = "okay";
​
			port {
					panel_in: endpoint {
							remote-endpoint = <&dsi0_out>;
					};
			};
	};
};
  • Configure pins
&pinctrl {
	du_pins: du {
		data {
			pinmux = <RZG2L_PORT_PINMUX(7,  2, 1)>,
				 <RZG2L_PORT_PINMUX(8,  0, 1)>,
				 <RZG2L_PORT_PINMUX(8,  1, 1)>,
				 <RZG2L_PORT_PINMUX(8,  2, 1)>,
				 <RZG2L_PORT_PINMUX(9,  0, 1)>,
				 <RZG2L_PORT_PINMUX(9,  1, 1)>,
				 <RZG2L_PORT_PINMUX(10, 0, 1)>,
				 <RZG2L_PORT_PINMUX(10, 1, 1)>,
				 <RZG2L_PORT_PINMUX(11, 0, 1)>,
				 <RZG2L_PORT_PINMUX(11, 1, 1)>,
				 <RZG2L_PORT_PINMUX(12, 0, 1)>,
				 <RZG2L_PORT_PINMUX(12, 1, 1)>,
				 <RZG2L_PORT_PINMUX(13, 0, 1)>,
				 <RZG2L_PORT_PINMUX(13, 1, 1)>,
				 <RZG2L_PORT_PINMUX(13, 2, 1)>,
				 <RZG2L_PORT_PINMUX(14, 0, 1)>,
				 <RZG2L_PORT_PINMUX(14, 1, 1)>,
				 <RZG2L_PORT_PINMUX(15, 0, 1)>,
				 <RZG2L_PORT_PINMUX(15, 1, 1)>,
				 <RZG2L_PORT_PINMUX(16, 0, 1)>,
				 <RZG2L_PORT_PINMUX(16, 1, 1)>,
				 <RZG2L_PORT_PINMUX(17, 0, 1)>,
				 <RZG2L_PORT_PINMUX(17, 1, 1)>,
				 <RZG2L_PORT_PINMUX(17, 2, 1)>;
		};

		sync {
			pinmux = <RZG2L_PORT_PINMUX(6, 1, 1)>, /* HSYNC */
				 <RZG2L_PORT_PINMUX(7, 0, 1)>; /* VSYNC */
		};

		de {
			pinmux = <RZG2L_PORT_PINMUX(7, 1, 1)>; /* DE */
		};
		
		clk {
			pinmux = <RZG2L_PORT_PINMUX(6, 0, 1)>; /* CLK */
		};
	};
};


  • Add a rgb-dummy device
	rgb-dummy {
		compatible = "renesas,rgb-dummy";
		ports {
			#address-cells = <1>;
			#size-cells = <0>;

			port@0 {
				reg = <0>;
				rgb_in: endpoint {
					remote-endpoint = <&du_out_rgb>;
					};
				};
				port@1 {
					reg = <1>;
						rgb_out: endpoint {
							remote-endpoint = <&panel_in>;
						};
				};
			};
		};
  • Add panel device node:
panel {
	/* 
	* Define code for panel here such as compatible, backlight, power,...
	* Can refer drivers/gpu/drm/panel/panel-simple.c
	*/
	port {
		panel_in: endpoint {
			remote-endpoint = <&rgb_out>;
		};
	};
};


  • We want the MIPI DSI driver disabled
&dsi0 {
	status = "disabled";
};
  • Add endpoint for DU RGB out:
&du {
	pinctrl-0 = <&du_pins>;
	pinctrl-names = "default";

	ports {
		port@0 {
			du_out_rgb: endpoint {
				remote-endpoint = <&rgb_in>;
			};
		};
	};
 };


Audio

 

Linux Drivers

  • RZ/G2H, G2M, G2N, G2E: rz_linux-cip/sound/soc/sh/rcar/*.c
  • RZ/G2L, G2LC, G2UL, V2L: rz_linux-cip/sound/soc/sh/rz-ssi.c

Device Tree Examples

Here is an example of a MAX9867 on SSI channel 3, using I2C-3. MAX98390 Amplifier on I2C-2.

This is for the Linux-5.10 kernel. For the older Linux-4.19 kernel, there are some differences.

Pin Setup

&pinctrl {

	/* MAX98390 Amplifier */
	i2c2_pins: i2c2 {
		pinmux = <RZG2L_PORT_PINMUX(42, 3, 1)>, /* SDA */
			 <RZG2L_PORT_PINMUX(42, 4, 1)>; /* SCL */
	};

	/* MAX9867 Codec */
	i2c3_pins: i2c3 {
		pinmux = <RZG2L_PORT_PINMUX(18, 0, 3)>, /* SDA */
			 <RZG2L_PORT_PINMUX(18, 1, 3)>; /* SCL */
	};

	ssi3_pins: ssi3 {
	pinmux = <RZG2L_PORT_PINMUX(31, 0, 5)>, /* BCK */
		<RZG2L_PORT_PINMUX(31, 1, 5)>, /* RCK */
		<RZG2L_PORT_PINMUX(32, 0, 5)>, /* TXD */
		<RZG2L_PORT_PINMUX(32, 1, 5)>; /* RXD */
	};
};

Enable SSI channel

&ssi3 {
	pinctrl-0 = <&ssi3_pins>;
	pinctrl-names = "default";

	#sound-dai-cells = <1>;
	status = "okay";
};

Create a node for the MAX9867

	my_snd: sound {
		compatible = "simple-audio-card";
		simple-audio-card,widgets = "Speaker", "Ext Spk";

		simple-audio-card,routing =
		"Ext Spk", "BE_OUT";
		"Ext Spk", "LOUT",
		"Ext Spk", "ROUT";

		/* MAX98390 Amplifier */
		simple-audio-card,dai-link@0{
			format = "i2s";
			bitclock-master = <&cpu_dai3>;
			frame-master = <&cpu_dai3>;
			mclk-fs = <256>;
			cpu_dai3: cpu {
				sound-dai = <&ssi3>;
			};

			codec_dai3: codec {
				sound-dai = <&max98390>;
				clocks = <&mclk>;
			};
		};

		/* MAX9867 Codec */
		simple-audio-card,dai-link@1{
			format = "i2s";
			bitclock-master = <&cpu_dai0>;
			frame-master = <&cpu_dai0>;
			mclk-fs = <256>;
			cpu_dai0: cpu {
				sound-dai = <&ssi0>;
			};

			codec_dai0: codec {
				sound-dai = <&max9867>;
				clocks = <&mclk>;
			};
		};
	};


I2C node for the Codec and Amp

&i2c2 {
	pinctrl-0 = <&i2c2_pins>;
	pinctrl-names = "default";

	status = "okay";
	clock-frequency = <400000>;

	/* MAX98390 Amplifier */
	max98390: codec@3d {
		status = "okay";
		compatible = "maxim,max98390";
		#sound-dai-cells = <0>;
		reg = <0x3d>;
	};
};

&i2c3 {
	pinctrl-0 = <&i2c3_pins>;
	pinctrl-names = "default";

	status = "okay";
	clock-frequency = <400000>;

	/* MAX9867 Codec */
	max9867: codec@18 {
		status = "okay";
		compatible = "maxim,max9867";
		#sound-dai-cells = <0>;
		reg = <0x18>;
	};
};



Camera

Linux Drivers

  • RZ/G2H, G2M, G2N, G2E:
    • CONFIG_xxx=y
  • RZ/G2L, G2LC, G2UL, V2L:
    • CONFIG_xxx=y

Notes

Device Tree Examples

  • (see device tree for evaluation board)


Ethernet

 

Linux Drivers

  • RZ/G2H, G2M, G2N, G2E, G2L, G2LC, G2UL, V2L:
    • rz_linux-cip/drivers/net/ethernet/renesas/ (ravb_main.c, ravb_ptp.c)
    • Documentation/devicetree/bindings/net/renesas,etheravb.yaml
    • CONFIG_NET_VENDOR_RENESAS=y
    • # CONFIG_SH_ETH is not set
    • CONFIG_RAVB=y

Notes

  • The Link Status input pin (LINKSTA) is not used. The driver instead relies on the PHY to inform it that the link is up by using in-band status messages on the RGMII lines.
  • Do not forget to set the correct voltage levels for the pins (3.3v, 1.5v, etc..) in the device tree in the pinctrl node.
    • You use the syntax "power-source = <3300>;" when you declare the pins for Ethernet.
    • Refer to the pinctrl documentation in the kernel for more info.
    • Documentation/devicetree/bindings/pinctrl/renesas,rzg2l-pinctrl.yaml
    • Documentation/devicetree/bindings/pinctrl/renesas,pcf.yaml
  • In the Device Tree, the MDIO address is set by @x and the "reg =<x>;" For example, MDIO address of 0:
	phy0: ethernet-phy@0 {
		reg = <0>;

Device Tree Examples

Ethernet node for MII mode

&eth0 {
	pinctrl-0 = <&eth0_mii_pins>;
	pinctrl-names = "default";
	phy-handle = <&phy0>;
	phy-mode = "mii";
	status = "okay";

	phy0: ethernet-phy@7 {
		compatible = "ethernet-phy-id0022.1640",
			     "ethernet-phy-ieee802.3-c22";
		reg = <7>;
		rxc-skew-psec = <2400>;
		txc-skew-psec = <2400>;
		rxdv-skew-psec = <0>;
		txdv-skew-psec = <0>;
		rxd0-skew-psec = <0>;
		rxd1-skew-psec = <0>;
		rxd2-skew-psec = <0>;
		rxd3-skew-psec = <0>;
		txd0-skew-psec = <0>;
		txd1-skew-psec = <0>;
		txd2-skew-psec = <0>;
		txd3-skew-psec = <0>;

		interrupt-parent = <&pinctrl>;
		interrupts = <RZG2L_GPIO(1, 0) IRQ_TYPE_LEVEL_LOW>;
	};
};

&eth1 {
	pinctrl-0 = <&eth1_mii_pins>;
	pinctrl-names = "default";
	phy-handle = <&phy1>;
	phy-mode = "mii";
	status = "okay";

	phy1: ethernet-phy@7 {
		compatible = "ethernet-phy-id0022.1640",
			     "ethernet-phy-ieee802.3-c22";
		reg = <7>;
		rxc-skew-psec = <2400>;
		txc-skew-psec = <2400>;
		rxdv-skew-psec = <0>;
		txdv-skew-psec = <0>;
		rxd0-skew-psec = <0>;
		rxd1-skew-psec = <0>;
		rxd2-skew-psec = <0>;
		rxd3-skew-psec = <0>;
		txd0-skew-psec = <0>;
		txd1-skew-psec = <0>;
		txd2-skew-psec = <0>;
		txd3-skew-psec = <0>;

		interrupt-parent = <&pinctrl>;
		interrupts = <RZG2L_GPIO(1, 1) IRQ_TYPE_LEVEL_LOW>;
	};
};


Pin Setup

&pinctrl {

	eth0_mii_pins: eth0 {
		pinmux = <RZG2L_PORT_PINMUX(28, 1, 1)>, /* ET0_LINKSTA */
			 <RZG2L_PORT_PINMUX(27, 1, 1)>, /* ET0_MDC */
			 <RZG2L_PORT_PINMUX(28, 0, 1)>, /* ET0_MDIO */
			 <RZG2L_PORT_PINMUX(20, 0, 1)>, /* ET0_TXC */
			 <RZG2L_PORT_PINMUX(20, 1, 1)>, /* ET0_TX_CTL */
			 <RZG2L_PORT_PINMUX(20, 2, 1)>, /* ET0_TXD0 */
			 <RZG2L_PORT_PINMUX(21, 0, 1)>, /* ET0_TXD1 */
			 <RZG2L_PORT_PINMUX(21, 1, 1)>, /* ET0_TXD2 */
			 <RZG2L_PORT_PINMUX(22, 0, 1)>, /* ET0_TXD3 */
			 <RZG2L_PORT_PINMUX(22, 1, 1)>,	/* ETH0_TX_ERR */
			 <RZG2L_PORT_PINMUX(23, 0, 1)>,	/* ETH0_TX_COL */
			 <RZG2L_PORT_PINMUX(23, 1, 1)>, /* ETH0_TX_CRS */
			 <RZG2L_PORT_PINMUX(24, 0, 1)>, /* ET0_RXC */
			 <RZG2L_PORT_PINMUX(24, 1, 1)>, /* ET0_RX_CTL */
			 <RZG2L_PORT_PINMUX(25, 0, 1)>, /* ET0_RXD0 */
			 <RZG2L_PORT_PINMUX(25, 1, 1)>, /* ET0_RXD1 */
			 <RZG2L_PORT_PINMUX(26, 0, 1)>, /* ET0_RXD2 */
			 <RZG2L_PORT_PINMUX(26, 1, 1)>, /* ET0_RXD3 */
			 <RZG2L_PORT_PINMUX(27, 0, 1)>; /* ETH0_RX_ERR */
	};

	eth1_mii_pins: eth1 {
		pinmux = <RZG2L_PORT_PINMUX(37, 2, 1)>, /* ET1_LINKSTA */
			 <RZG2L_PORT_PINMUX(37, 0, 1)>, /* ET1_MDC */
			 <RZG2L_PORT_PINMUX(37, 1, 1)>, /* ET1_MDIO */
			 <RZG2L_PORT_PINMUX(29, 0, 1)>, /* ET1_TXC */
			 <RZG2L_PORT_PINMUX(29, 1, 1)>, /* ET1_TX_CTL */
			 <RZG2L_PORT_PINMUX(30, 0, 1)>, /* ET1_TXD0 */
			 <RZG2L_PORT_PINMUX(30, 1, 1)>, /* ET1_TXD1 */
			 <RZG2L_PORT_PINMUX(31, 0, 1)>, /* ET1_TXD2 */
			 <RZG2L_PORT_PINMUX(31, 1, 1)>, /* ET1_TXD3 */
			 <RZG2L_PORT_PINMUX(32, 0, 1)>, /* ETH1_TX_ERR */
			 <RZG2L_PORT_PINMUX(32, 1, 1)>, /* ETH1_TX_COL */
			 <RZG2L_PORT_PINMUX(33, 0, 1)>, /* ETH1_TX_CRS */
			 <RZG2L_PORT_PINMUX(33, 1, 1)>, /* ET1_RXC */
			 <RZG2L_PORT_PINMUX(34, 0, 1)>, /* ET1_RX_CTL */
			 <RZG2L_PORT_PINMUX(34, 1, 1)>, /* ET1_RXD0 */
			 <RZG2L_PORT_PINMUX(35, 0, 1)>, /* ET1_RXD1 */
			 <RZG2L_PORT_PINMUX(35, 1, 1)>, /* ET1_RXD2 */
			 <RZG2L_PORT_PINMUX(36, 0, 1)>, /* ET1_RXD3 */
			 <RZG2L_PORT_PINMUX(36, 1, 1)>; /* ETH1_RX_ERR */
	};
};  

USB

Linux Drivers

  • RZ/G2H, G2M, G2N, G2E:
  • RZ/G2L, G2LC, G2UL, V2L:

Host

  • (uses standard EHCI and XHCI kernel drivers since H/W API is fixed)
  • drivers/usb/host/ehci-hcd.c
  • drivers/usb/host/ehci-platform.c
  • drivers/usb/host/xhci.c
  • drivers/usb/host/xhci-rcar.c
    • CONFIG_USB_EHCI_HCD=y
    • CONFIG_XHCI_PLATFORM=y
    • CONFIG_XHCI_RCAR=y

Device

  • drivers/usb/renesas_usbhs/*
    • USB_RENESAS_USBHS=y

PHY

  • The PHY is a separate H/W block. Also used to control host/device switching for OTG.
  • drivers/phy/renesas/*
    • CONFIG_PHY_RCAR_GEN3_USB2=y
    • CONFIG_PHY_RCAR_GEN3_USB3=y

Notes

  • Disable OverCurrent Protection Interrupts:

If you did not connect the USB_OVCUR pin on your board, and it floats, you will get interrupt messages about over current. However, you can disable this interrupt by modifying the setting for the OHCI HcRhDescriptorA Register and setting bit NOCP to '1'. Search for "HcRhDescriptorA" in the hardware manual for more information.In the kernel, in file drivers/usb/host/ohci-hcd.c, you want to comment out the line:/* Configure for per-port over-current protection by default */val &= ~RH_A_NOCP;In u-boot, can see this is sometimes done for Renesas boards. See file board/renesas/rzg2l-dev/rzg2l-dev.c(*(volatile u32 *)(USB1_BASE + HcRhDescriptorA)) |= (0x1u << 12); /* NOCP = 1 */

  • Dynamic changing from Device and Host for OTG:

If you are using a device as OTG (On-the-Go) and want to change from device to you, you set a sysfs setting under the PHY driver (not the USB controller driver)$ echo host > /sys/devices/platform/soc/ee080200.usb-phy/role


Device Tree Examples

  • (see device tree for evaluation board)

SD Card


Linux Drivers

  • RZ/G2H, G2M, G2N, G2E:
    • CONFIG_xxx=y
  • RZ/G2L, G2LC, G2UL, V2L:
    • CONFIG_xxx=y

Notes

  • Same as eMMC: The drivers for SD Card and SDIO are the same as eMMC. Please the section on eMMC.
  • 3.3v Only: If you only provide 3.3v (do not support dynamically switching to 1.8v for UHS), then you should add the no-1-8-v; flag to the sdhi node. This flag is used for both kernel and u-boot device trees.
  • vmmc-supply: This is the voltage regulator connected to the SD card VDD pin. It could be a constant fixed 3.3v, or it be attached to a regulator that you can turn off to save power.
  • vqmmc-supply: This is the voltage regulator that the pull-ups for the data lines go to. For high speed SD, they will change from 3.3v to 1.8v.

Device Tree Examples

  • (see device tree for evaluation board)
/ {
	reg_3p3v: regulator1 {
		compatible = "regulator-fixed";

		regulator-name = "fixed-3.3V";
		regulator-min-microvolt = <3300000>;
		regulator-max-microvolt = <3300000>;
		regulator-boot-on;
		regulator-always-on;
	};

	vccq_sdhi1: regulator-vccq-sdhi1 {
		compatible = "regulator-gpio";
		regulator-name = "SDHI1 VccQ";
		regulator-min-microvolt = <1800000>;
		regulator-max-microvolt = <3300000>;
		gpios-states = <1>;
		states = <3300000 1>, <1800000 0>;
	};
};

&sdhi1 {
	pinctrl-0 = <&sdhi1_pins>;
	pinctrl-1 = <&sdhi1_pins_uhs>;
	pinctrl-names = "default", "state_uhs";

	vmmc-supply = <&reg_3p3v>;
	vqmmc-supply = <&vccq_sdhi1>;
	bus-width = <4>;
	sd-uhs-sdr50;
	sd-uhs-sdr104;
	status = "okay";
};


eMMC

Linux Drivers

  • RZ/G2H, G2M, G2N, G2E:
  • RZ/G2L, G2LC, G2UL, V2L:
    • driver/mmc/host/renesas_sdhi.h
    • driver/mmc/host/renesas_sdhi_core.c
    • driver/mmc/host/renesas_sdhi_internal_dmac.c
    • driver/mmc/host/tmio_mmc.h
    • driver/mmc/host/tmio_mmc_core.c
    • CONFIG_MMC_SDHI=y
    • CONFIG_MMC_SDHI_INTERNAL_DMAC=y (selected automatically by MMC_SDHI)
    • CONFIG_MMC_TMIO_CORE=y (selected automatically by MMC_SDHI)

Notes

  • Combo driver for MMC + SDHI HW
  • The core of the SDHI code is using the TMIO (Toshiba Mobile IO) driver because it is the same HW block and they have shared the same driver for many years.
  • CONFIG_MMC_SDHI_SYS_DMAC=y is selected automatically by MMC_SDHI, but is only for RZ/G1 series devices.
  • Note that if you are using more than one mmc/sdhi channel, you might run into the issue that you don't get the same device number (ie, /dev/mmcblk0) each time you boot. To fix this, simply add an 'alias' to the top of your Device Tree to make each channel a fixed number. As an example:
	aliases {
		mmc0 = &sdhi3; // eMMC Flash for rootfs
		mmc1 = &sdhi0; // SD Card Socket
		mmc2 = &sdhi2; // SDIO for WiFi
	};

Device Tree Examples

  • (see device tree for evaluation board)

DMA

Linux Drivers

  • RZ/G2H, G2M, G2N, G2E:
    • drivers/dma/sh/*
    • CONFIG_RCAR_DMAC=y
  • RZ/G2L, G2LC, G2UL, V2L:
    • drivers/dma/sh/rz-dma.c
    • CONFIG_RZ_DMAC=y

Notes

RZ/G2L, RZ/V2L, How to determine 'dmas' value

  • Given the Device Tree example below for SPI-1, you will need to determine the values for the "tx" and "rx" DMA triggers.
&spi1 { 
      pinctrl-0 = <&spi1_pins>;
      pinctrl-names = "default";
      dmas = <&dmac  0x2e99 >, <&dmac  0x2e9a >;
      dma-names = "tx", "rx";
      status = "okay";
};
  • You can find some explanation in the kernel documentation: Documentation/devicetree/bindings/dma/renesas,rz-dmac.yaml
  '#dma-cells':
    const: 1
    description:
      The cell specifies the encoded MID/RID values of the DMAC port
      connected to the DMA client and the slave channel configuration
      parameters.
      bits[0:9] - Specifies MID/RID value
      bit[10] - Specifies DMA request high enable (HIEN)
      bit[11] - Specifies DMA request detection type (LVL)
      bits[12:14] - Specifies DMAACK output mode (AM)
      bit[15] - Specifies Transfer Mode (TM)
  • These values are what get written directly to the DMA registers. Also, the values for these bits are fixed and shown in a table in the hardware manual.
  • If you look in the Direct Memory Access Control (DMA) chapter in the hardware manual, you will find the table "On-Chip Module Requests"

Example: RZ/G2L RSPI ch1

RZG2L DMA Request Table SPI.png

SPIT1 (tranmit buffer empty) dma-names = "tx"

  MID[7:0] = 10100110'b
  RID[1:0] = 01'b
  HEIN = 1'b
  LVL = 1'b
  AM[2:0] = 010'b
  TM = 0'b

  AM    HEIN       RID
  |     |          |
0 010 1 1 10100110 01 = 0010 1110 1001 1001 =  0x2e99 
|     |   |
TM    LVL MID


SPIR1 (receive buffer full) dma-names = "rx"

  MID[7:0] = 10100110'b
  RID[1:0] = 10'b
  HEIN = 1'b
  LVL = 1'b
  AM[2:0] = 010'b
  TM = 0'b

  AM    HEIN       RID
  |     |          |
0 010 1 1 10100110 10 = 0010 1110 1001 1010 =  0x2e9a 
|     |   |
TM    LVL MID

Device Tree Examples

  • (see device tree for evaluation board)



I2C

Linux Drivers

  • RZ/G2H, G2M, G2N, G2E:
    • CONFIG_xxx=y
  • RZ/G2L, G2LC, G2UL, V2L:
    • drivers/i2c/busses/ i2c-riic.c
    • CONFIG_I2C_RIIC=y

Notes

Device Tree Examples

  • (see device tree for evaluation board)

SPI

Linux Drivers

  • MSIOF: RZ/G2H, G2M, G2N, G2E:
    • CONFIG_xxx=y
  • RSPI: RZ/G2L, G2LC, G2UL, V2L:
    • drivers/spi/spi-rspi.c
    • CONFIG_SPI_RSPI=y

Notes

  • spidev:
    • If you want a generic SPI device (/dev/spi-0), in the past you would allocate a compatible = "spidev"; node. Unfortunately, that spidev name has been removed from Linux (since Linux-5.17). However, you can still create a spidev device by simply using another name that is already in the kernel. The compatible name will be different, but it will work the exact same way.
    • Below is the list of device that can be used with spidev from file drivers/spi/spidev.c

static const struct of_device_id spidev_dt_ids[] = { { .compatible = "rohm,dh2228fv" }, { .compatible = "lineartechnology,ltc2488" }, { .compatible = "ge,achc" }, { .compatible = "semtech,sx1301" }, { .compatible = "lwn,bk4" }, { .compatible = "dh,dhcom-board" }, { .compatible = "menlo,m53cpld" }, {}, };

For example, if you just pick the first name in the list ("rohm,dh2228fv") this will work on any kernel version:&spi1 { pinctrl-0 = <&spi1_pins>; pinctrl-names = "default"; status = "okay"; dmas = <&dmac 0x2e99>, <&dmac 0x2e9a>; dma-names = "tx", "rx"; spidev@0{ compatible = "rohm,dh2228fv"; // (Using fake name to use spidev driver) reg = <0>; spi-max-frequency = <1000000>; }; };

Device Tree Examples

  • (see device tree for evaluation board)

QSPI Flash

Linux Drivers

  • RZ/G2H, G2M, G2N, G2E:
    • drivers/spi/spi-rpc-if.c
    • drivers/memory/renesas-rpc-if.c
    • drivers/mtd/hyperbus/rpc-if.c
    • CONFIG_SPI_RPCIF=y
    • CONFIG_RENESAS_RPCIF=y
    • CONFIG_RPCIF_HYPERBUS=y
  • RZ/G2L, G2LC, G2UL, V2L:
    • CONFIG_xxx=y

Notes

  • unrecognized JEDEC id bytes: If when booting the kernel, you get a message like:
[    2.328844] rpc-if-spi rpc-if-spi: registered master spi2
[    2.328891] spi spi2.0: setup mode 0, 8 bits/w, 50000000 Hz max --> 0
[    2.329230] spi-nor spi2.0: unrecognized JEDEC id bytes: 1f 87 01 1f 87 01

it means this nor flash is not supported in the Linux kernel. To support this flash, you should add this flash info in "static const struct flash_info atmel_parts[]" in drivers/mtd/spi-nor/atmel.c:

{ "at25sf321", INFO(0x1f8701, 0, 64 * 1024, 64, SECT_4K | SPI_NOR_DUAL_READ | SPI_NOR_QUAD_READ) },

Device Tree Examples

  • (see device tree for evaluation board)

UART (SCIF)

Linux Drivers

  • RZ/G2H, G2M, G2N, G2E:
    • CONFIG_xxx=y
  • RZ/G2L, G2LC, G2UL, V2L:
    • CONFIG_xxx=y

Notes

Device Tree Examples

  • (see device tree for evaluation board)

UART (SCI)

Linux Drivers

  • RZ/G2H, G2M, G2N, G2E:
    • CONFIG_xxx=y
  • RZ/G2L, G2LC, G2UL, V2L:
    • CONFIG_xxx=y

Notes

Device Tree Examples

  • (see device tree for evaluation board)

CAN

Linux Drivers

  • RZ/G2H, G2M, G2N, G2E:
  • RZ/G2L, G2LC, G2UL, V2L:
    • drivers/net/can/rcar/*
    • CONFIG_CAN_RCAR=y
    • CONFIG_CAN_RCAR_FD=y

Notes

  • CAN-FD is enabled by default. To switch to CAN protocol, a user can add property "renesas,no-can-fd" in the Device Tree

Device Tree Examples

  • (see device tree for evaluation board)

ADC

Linux Drivers

  • RZ/G2H, G2M, G2N, G2E:
    • CONFIG_xxx=y
  • RZ/G2L, G2LC, G2UL, V2L:
    • CONFIG_xxx=y

Notes

Device Tree Examples

  • (see device tree for evaluation board)

Watchdog Timer(WDT)

Linux Drivers

  • RZ/G2H, G2M, G2N, G2E:
    • rz_linux-cip/drivers/watchdog/renesas_wdt.c
    • CONFIG_RENESAS_WDT
  • RZ/G2L, G2LC, G2UL, V2L:
    • rz_linux-cip/drivers/watchdog/rzg2l_wdt.c
    • CONFIG_RENESAS_RZG2LWDT

Notes

  • When rebooting the system, the watchdog timer is used. Simply type the command line "reboot" in the console.
  • To test a watch dog timeout/reboot, enter this command in the console "cat >> /dev/watchdog", then press ENTER again, then wait 1 minutes, and the board should reboot.
  • RZ/G2L: Reset on a WDT Timeout: There is a register in the CPG (WDT Reset Selector Register - CPG_WDTRST_SEL) to control if the WDT will reset the system or not. To generate a system RESET, you need to set it to 0x00010001. You can do this in u-boot, or when the kernel boots (in the CPG driver, not the WDT driver).
# Add this code to u-boot

#define CPG_WDTRST_SEL    (CPG_BASE + 0xB14)
*(volatile u32 *)(CPG_WDTRST_SEL) = 0x00010001;

 - or - 

# Add this code to the kernel CPG driver
  # FILE: drivers/clk/renesas/rzg2l-cpg.c
  # FUNCTION: rzg2l_cpg_probe()
  # LINE: Before the 'return 0;' at the end of the funtion

writel(0x00010001, (priv->base + 0xB14));

  • RZ/G2L: Toggle WDTOVF_PERROUT# Note that by default, the WDTOVF_PERROUT# pin will not toggle on a WDT reboot. You need to set the CPG_WDTRST_SEL register manually in u-boot since Linux never touches that register. For example:
#define CPG_WDTRST_SEL    (CPG_BASE + 0xB14)
*(volatile u32 *)(CPG_WDTRST_SEL) = 0x00100010;

Device Tree Examples

  • (see device tree for evaluation board)

PWM

Linux Drivers

  • RZ/G2H, G2M, G2N, G2E:
    • CONFIG_xxx=y
  • RZ/G2L, G2LC, G2UL, V2L:
    • CONFIG_xxx=y

Notes

Device Tree Examples

  • (see device tree for evaluation board)


Timer

Linux Drivers

  • RZ/G2H, G2M, G2N, G2E:
    • CONFIG_xxx=y
  • RZ/G2L, G2LC, G2UL, V2L:
    • CONFIG_xxx=y

Notes

Device Tree Examples

  • (see device tree for evaluation board)

Thermal

Linux Drivers

  • RZ/G2H, G2M, G2N, G2E:
    • drivers/thermal/rcar_gen3__thermal.c
    • CONFIG_RCAR_GEN3_THERMAL=y
  • RZ/G2L, G2LC, G2UL, V2L:
    • drivers/thermal/rzg2l_thermal.c
    • CONFIG_RZG2L_THERMAL=y

Notes

  • The Linux driver reads the registers and applies the formula in the hardware manual
  • You can read the current value running the command:
    • $ cat /sys/class/thermal/thermal_zone0/temp
  • The output value is in millicelsius

Device Tree Examples

  • (see device tree for evaluation board)

PMIC RAA215300

Linux Drivers

    • drivers/mfd/raa215300.c
    • CONFIG_PMIC_RAA215300=y
    • Documentation/devicetree/bindings/mfd/raa215300.txt

Notes

  • Only supports RTC function
  • Added in VLP/G v3.0.1 release (branch rz-5.10-cip13)

Device Tree Examples

  • (see device tree for evaluation board)
  • No labels