You are viewing an old version of this page. View the current version.
Compare with Current View Page History
« Previous Version 4 Current »
1. Download the Linux BSP
2. Build Environment
⚠️ The BSP will only build in Ubuntu 20.04
3. Build the BSP
4. Prepare an SD Card
5. Boot the Board
RZ/G2 Group Application Note and Source Codes of Sample Applications
RZ/G2 Door Phone Demo
HiHope Device Tree files are located in Yocto under:
build/tmp/work-shared/hihope-rzg2m/kernel-source/arch/arm64/boot/dts/renesas/
NOTE: The file names below are for RZ/G2M (r8a774a1-hihope-rzg2m.dts), but the same applies for RZ/G2N and RZ/G2H Device Tree files.
If you have a sub-board attached (with the Ethernet connector), then you should use the "-ex" versions of the Device Tree.
Starting with VLP64 v1.0.4, the default Device Tree file will be for HiHope boards HIHOPE_RZ/G2_V3 boards or later.
You can find the version of your board printed on both the main board and sub-board.
Boards V3 or later
If you are using an older V2 board, then you will need to use the "-rev2" Device Tree Files.
Board V2 only
You need to add 2 new nodes in the Device Tree: One in the ‘pfc’ section to configure pin muxing, and another node at the global level to enable to I2C peripheral interface.
Edit the file:
build/tmp/work-shared/hihope-rzg2m/kernel-source/arch/arm64/boot/dts/renesas/r8a774a1-hihope-rzg2m-ex.dts
and at the end of the file, add the following:
/* * Enable I2C0 on CN1801 * GP3_14 = scl0 * GP3_15 = sda0 */ &pfc { i2c0_pins: i2c0 { groups = "i2c0"; function = "i2c0"; }; }; &i2c0 { pinctrl-0 = <&i2c0_pins>; pinctrl-names = "default"; status = "okay"; clock-frequency = <100000>; };
You can change the clock-frequency to 400000 if you like.
To rebuild the Device Tree:
1. Run this bitbake command:
bitbake -c devshell linux-renesas
2. This will open a new window. In the new window, run:
make dtbs exit
3. Now to repackage and copy the files into the 'deploy' directory, run this bitbake command:
bitbake linux-renesas -f -c deploy
4. Copy your new .dtb file to your SD card and boot. Then you should see the device /dev/i2c-0
5. If you have i2c-tools installed, you can use i2cdetect to confirm your device is accessible. For example:
root$ i2cdetect -y -r 0 0 1 2 3 4 5 6 7 8 9 a b c d e f 00: -- -- -- -- -- -- -- -- -- -- -- -- -- 10: -- -- -- -- -- -- -- -- -- -- -- -- -- -- -- -- 20: -- -- -- -- -- -- -- -- -- -- -- -- -- -- -- -- 30: -- -- -- -- -- -- -- -- -- -- -- -- -- -- -- -- 40: -- -- -- -- -- -- -- -- -- -- 4a -- -- -- -- -- 50: -- -- -- -- -- -- -- -- -- -- -- -- -- -- -- -- 60: -- -- -- -- -- -- -- -- -- -- -- -- -- -- -- -- 70: -- -- -- -- -- -- -- --
When you get the message:
No Boot 0x00000010 0x60018118 0x00000008
If a prohibited setting is made in the Boot Mode setting, it will result in a No Boot state.
On the HiHope-RZG2M board, the same error occurs when the following DIP SW settings are made. 0x60018118 indicates the value of Mode Monitor Register (MODEMR).
0x60018118
MD8 MD7 MD6 MD5 MD4 MD3 MD2 MD1 MD0 1 0 0 0 1 1 0 0 0
Since MD5=0 is prohibited, it must be changed to MD5=1.
For eMMC Boot operation, it is necessary to change to MD1=1.
The u-boot for the RZ/G2 configures the HW (peripherals and drivers) in multiple locations.
Board | Device Tree | Header | Code |
RZ/G2M HiHope | arch/arm/dts/r8a774a1.dtsi arch/arm/dts/hihope-common.dtsi arch/arm/dts/r8a774a1-hihope-rzg2m.dts arch/arm/dts/r8a774a1-hihope-rzg2m-u-boot.dts | include/configs/hihope-rzg2m.h | board/renesas/hihope-rzg2m/hihope-rzg2m.c |
RZ/G2N HiHope | arch/arm/dts/r8a774b1.dtsi arch/arm/dts/hihope-common.dtsi arch/arm/dts/r8a774b1-hihope-rzg2n.dts arch/arm/dts/r8a774b1-hihope-rzg2n-u-boot.dts | include/configs/hihope-rzg2n.h | board/renesas/hihope-rzg2n/hihope-rzg2n.c |
RZ/G2N HiHope | arch/arm/dts/r8a774e1.dtsi arch/arm/dts/hihope-common.dtsi arch/arm/dts/r8a774e1-hihope-rzg2h.dts arch/arm/dts/r8a774e1-hihope-rzg2h-u-boot.dts | include/configs/hihope-rzg2h.h | board/renesas/hihope-rzg2n/hihope-rzg2h.c |