You are viewing an old version of this page. View the current version.

Compare with Current View Page History

Version 1 Current »

The RZ/V Series has two version of the Image Signal Processor (ISP)

RZ/V2L Simple ISP Support Package

RZV/2M Full ISP Support Package

RZ/V2L Simple ISP (Memory)

The Simple ISP uses a working memory area for processing camera streams. This working memory area is defined in the device memory space define ISP Reserved memory area ( see Figure ). In the Application Layer uses the Video 4 Linux API (VIDIOC_REQBUFS, VIDIOC_QUERYBUF) to allocated memory. How much of this memory is used is defined by the camera device resolution, pixel color depth, and capture frame buffer count. The ISP revered memory space is defined in the RZV2L Linux Device Tree File ( r9a07g04512-smarc.dts ).

RZV2L BSP v1.0.1 Memory Map ( RZ/V2L Linux Package V1.0.1 Release Note )

BSP v1.01 file : r9a07g054l2-smarc.dts

isp_work0: SIMPLE_ISP {
	reusable;
	reg = <0x0 0xBD000000 0x0 0x03000000>;
};

RZV2L BSP v1.0.1 Memory Area

OV5645 Supported Resolutions
WidthHeightPixel DepthNumber FramesTotal Memory Usage
640480263,686,400
12807202611,059,200
192010802624,883,200
25921944 *12660,466,146 *2

1 ) Maximum Resolution for OV5645. For AI inference please uses smaller resolution.

2 ) Due to the BSP v1.0.1 ISP resaved area size ( 48MB ) this resolution is not supported. The reserved memory needs to be increased.

RZ/V2L Simple ISP Monitor Demo

RZ/V2L ISP Sample Camera Demo

This demo show how to implement the RZ/V2L Simple ISP with OV5645 Cameras. This expands on the RZ/V2L ISP Sample Application that is included with the RZ/V2L ISP Package with all the resolutions listed in the section above.

Run RZV2L Simple ISP Demos

Requirements
  • Linux BSP SDK : The SDK must include the DRP-AI and ISP packages. Refer to Linux BSP Release Note instructions (r01an6221ej<version>-rzv2l-linux.pdf) Section 6.
  • RZV2L DRP-AI Sample Application : ( rzv2l_drpai-sample-application_ver5.00.tar.gz )
  • Power : A powered hub or PC may not provide sufficient power. A USB Power Block is suggested.
Build ISP Monitoring Application

Detailed instructions for setup and building are located in the Application Note Revision documents in "Simple ISP Sample Application Note Revision" package.

  • ⚠️ You must first follow the Simple ISP Sample Application Note Revision instructions (r11an0563ej<version>-rzv2l-simple-isp.pdf) Section 2.0 and 2.6

These instructions are a summary of what is explained in the package Release Notes.

export ISP_FILE=r11an0561ej0100-rzv2l-isp-sp.zip

# Step 1. Extract the ISP package and ISP sample application files. Enter the ISP Montitoring source directory.
unzip $ISP_FILE -d isp_work
cd isp_work
tar zxvf rzv2l_isp-sample-application_ver1.00.tar.gz
cd app_isp_monitoring/src

# Step 2. Start the SDK
source /opt/poky/3.1.5/environment-setup-aarch64-poky-linux

# Step 3. Build the source with make
make



Build ISP Tiny YoloV2 Application

Detailed instructions for setup and building are located in the Application Note Revision documents in "Simple ISP Sample Application Note Revision" package.

  • ⚠️ You must first follow the Simple ISP Sample Application Note Revision instructions (r11an0563ej<version>-rzv2l-simple-isp.pdf) Section 2.0 and 2.7

This build requires the DRP-AI Tiny Yolo V2 Cam source is needed for this build ( /rzv2l_drpai-sample-application/app_tinyyolov2_cam/src ).

This build requires the DRP-AI Tiny Yolo V2 Cam directory "tinyyolov2_cam" is needed for this build ( /rzv2l_drpai-sample-application/app_tinyyolov2_cam/exe ).

These instructions are a summary of what is explained in the package Release Notes.

mkdir drp-ai-supporrt
export DRP_WORKDIR=$PWD/drp-ai-support

mkdir isp-support
export ISP_	WORKDIR=$PWD/isp-support

export APP_WORKDIR=$PWD

# Step 1. Extract the DRP Appicatiion Code to $DRP_WORK
unzip r11an0549ej0500-rzv2l-drpai-sp.zip -d $DRP_WORK
cd $DRP_WORK/rzv2l_drpai-sample-application/
tar -xvf rzv2l_drpai-sample-application_ver5.00.tar.gz -C .
cd $APP_WORKDIR

# Step 2. Extract the ISP Application Code to $ISP_WORK
unzip r11an0561ej0100-rzv2l-isp-sp.zip -d $ISP_WORK
cd $ISP_WORK
tar -xvf rzv2l_isp-sample-application_ver1.00.tar.gz -C .
cd $APP_WORKDIR


# Step 3. Copy TinyYoloV2 source code to ISP TinyYoloV2 application source directory
cp -r drp-ai-support/rzv2l_drpai-sample-application/app_tinyyolov2_cam/src/ ./isp-support/app_tinyyolov2_cam/src/

# Step 4. Apply Patch
cd $ISP_WORKDIR/app_tinyyolov2_cam/src/
patch -p 1 < rzv2l_app_tinyyolov2_cam_usb2mipi.patch

# Step 5. Setup SDK
source /opt/poky/3.1.5/environment-setup-aarch64-poky-linux

# Step . Build Source
make



RZ/V2M ISP usage

H.265/H.264 Multi Codec (VCD): How to start encoding after only 1 raw frame from the CSI camera

instead of using B_IMAGE_StartMovieStream, use these functions in the following order:

B_IMAGE_StartObjectToMovieStream

B_IMAGE_Imread

B_OBJ_BeginReadingData

B_IMAGE_EncodeRequestStream
  • No labels