You are viewing an old version of this page. View the current version.
Compare with Current View Page History
« Previous Version 3 Next »
Welcome to the Renesas Bluetooth® Low Energy MCU Wiki
This page is about the Renesas Bluetooth®® Low Energy devices. These are a set of Low Cost, Low Power SoC’s and Modules. The main goal of this page is to make the on-line information better accessible for HW and SW developers.
The Renesas.com website lists information per product; on this page we will present information per topic. We will go through a typical design cycle from Board availability, Getting Started guides till production line testing.
This page is meant to serve as a complementary resource available on Renesas web site for the Bluetooth® Low Energy SOCs.
For each of the Bluetooth® Low Energy products Renesas has 2 types of boards available:
Target device:
Each of the boards has a getting started guide available. The purpose of such a guide is to help users get a board up and running in as short as possible time. It will explain how to connect the hardware, Install the required SW packages, Compile a first Blinky code and Flash it into the target device.
The hardware design of battery supplied wireless products requires extra attention. Each of the products has a hardware guidelines document that explains what needs to be considered when designing schematic and layout of a product. Some products have schematics and layout examples available for download. Antenna design is generic for all BLE products. Different antenna topologies are explained in a dedicated document together with design files.
The respective Getting Started Guides explain which tools need to be installed for each device family. This section will summarize on the tools and list a couple of additional tools that are available.
Each of the BLE products comes with a Software Development Kit. This can be downloaded from the Renesas website after accepting a license agreement. Next to the Bluetooth stack and a few utilities, the SDK includes several application layer SW examples.
SDK10 (10.1.2.86) for DA14592
SDK and Platform Reference Manual
In addition to the SDK zip file developers can also make use of SW examples on Github. These examples demonstrate for instance the use of the low level drivers and also more complex Bluetooth use cases. There SW examples are created in a modular approach such that users can test and re-use them in their target application.
Next to the software examples the user can find useful information in a selection of on-line tutorials. Below is a list of Tutorials with short description:
DA14592
Title | Description |
---|---|
DA14592 Getting started | This tutorial is an introduction into SDK10. It explains how to implement basic functionality in the embedded firmware |
Software Platform Reference Manual | This document explains deeply the SDK |
Tutorial BLE Custom Service | Tutorial explaining what is a custom GATT profile and how to create one |
Tutorial Advertising Concepts | Tutorial describing how to create a BLE advertiser |
Tutorial Starting a Project | Explains how to start your first project on DA14592 and e2 Studio |
Title | Description |
---|---|
SDK6 Getting started | This tutorial is an introduction into SDK6. It explains how to implement basic functionality in the embedded firmware |
SDK6 peripheral drivers | This document provides info about the available low level drivers in the SDK and how to use them |
Booting from OTP and Serial | This document explains the various boot options from the external interface |
BLE advertiser | Tutorial describing how to create a BLE advertiser |
Create a custom GATT Profile | Tutorial explaining what is a custom GATT profile and how to create one |
BLE Sleep modes | Explains how to create a device with lowest possible power consumption |
BLE security | The tutorial gives basic understanding of BLE security and how to use this on SDK6 |
Flash selector Guide | An overview of Flash devices that has been verified for DA145xx and SDK6 |
Tutorial SW debugging | Tips and tricks on the various debugging techniques |
Title | Description |
---|---|
Starting a project | The tutorial explains how to start your own SDK10 project |
Using the Adapters in SDK10 | Using the I2C the Adapter concept is explained as used in SDK10 |
Booting from Serial interfaces | This document explains the various boot options from the UART or QSPI Flash |
BLE advertiser | Tutorial describing how to create a BLE advertiser |
Flash Driver Creation | How to develop a new custom QSPI driver for Flash or RAM |
Flash Adaptor for Data Storage | How to implement Non-Voltatile data storage using the available adapter |
How to use images bigger than 512 | Document explaining how to configure the SDK to run images larger than the default 512kB |
Power management | Tutorial explaining how to define hardware and software set-up for power consumption measurements |
Secure Boot Mechanism | The document explains how to use the feature of secure boot in the project |
Technical support discussions about Renesas BLE products, hardware, software can be found in the Renesas Engineering Community. You can also ask your question or report anything concerning this Wiki.
https://community.renesas.com/wireles-connectivity/f/bluetooth-low-energy