If you encounter any issues after the upgrade, please open a support request TICKET.🙌
Some RX MCU peripherals use only fixed interrupt vectors, while some others also use software configurable interrupt vectors.
The software configurable interrupt vectors can configure which interrupt is enable by user depending on the application.
It depends on which driver is used if you use a software configurable interrupt.
This is an example for GTCIU2 setting in GPT:
To resolve this error, you must configure additional interrupt settings in the "Interrupt tab".
As shown in the figure below, you need to select the interrupt from the corresponding interrupt vector group, INTA or INTB.
Please also refer to the "User Manual: Hardware" of each product to determine whether the interrupt belongs to INTA or INTB.
(see also the appendix of this page)
Please check the r_bsp_interrupt_config.h located in the src/smc_gen/r_config/.
If the software configurable interrupt setting is not applied correctly, the vector table may be set as blank.
Please check from this table in the Users manual: Hardware that you will use depens on the software configurable interrupt.