Overview
The Renesas TVM is the Extension package of Apache TVM Deep Learning Complier for Renesas DRP-AI accelerators powered by EdgeCortix MERA™. The TVM is a software framework that translates Neural Networks to run on the Renesas MPUs. While the AI Translator (see section above) can translate ONNX models to the DRP-AI hardware, it is restricted by the supported AI operations. This can restrict the number of supported AI Models. The TVM Translator expands the number of supported AI models for the RZV processors (currently RZV2L, RZV2MA, RZV2M). The TVM translates ONNX models by delegating the generated output between the DRP-AI and CPU.
This is the TVM Software framework based on the Apache TVM. The TVM includes python support libraries, and sample scripts. The python scripts follow the Apache TVM framework API found here.
- The TVM Provides the following
- Wider supported range of AI Networks that can run on the DRP-AI and CPU.
- Translate AI models from ONNX files
- Translate AI models from PyTorch PT saved models. ( For other supported AI Software Frameworks see Apache TVM)
- Translate models to run on CPU only. This allows models to run on RZG.
Official TVM Translator Github repo
Installation Directions Readme
Current Supported Renesas MPUs
- Renesas RZ/V2L Evaluation Board Kit
- Renesas RZ/V2M Evaluation Board Kit
- Renesas RZ/V2MA Evaluation Board Kit
Generated Output
BSP Supported Versions
Required VLP, DRP-AI and DRP-AI Translator are listed below. Board Support Package requirements can be found on the TVM repo page here.
RZV2H AI SDK is the recommended BSP. It includes VLP and DRP-AI Driver.
TVM | VLP (RZV2L) | VLP (RZV2M) | VLP (RZV2MA) | AI_SDK ( RZV2H ) | DRP-AI Driver RZVL,M.MA | DRP-AI Translator RZV2L,M,MA | DRP-AI Translator i8 RZV2H |
---|
v2.2.1 | v3.0.4 or later | v3.0.4 or later | v3.0.4 or later | v3.0.0 | v7.40 or later | v1.84 | v1.01 |
v2.2.0 | v3.0.4 or later | v3.0.4 or later | v3.0.4 or later | v3.0.0 | v7.40 or later | v1.83 | v1.01 |
v2.1.0 | v3.0.4 or later | v3.0.4 | v3.0.4 | v3.0.0 | v7.40 or later | v1.82 | v1.01 |
v1.1.1 | v3.0.4 | v3.0.4 | v3.0.4 |
| v7.40 | v1.82 | na |
v1,1.0 | v.3.0.2 | v1.3.0 update1 | v1.1.0 update1 |
| v7.30(V2L,M) v7.31(V2MA) | v1.82 | na |
v1.04 | v3.0.2 | v1.3.0 | v1.1.0 |
| v7.30 | v1.81 | na |
v1.03 | NS | NS | v1.0.0 |
| v7.20 | v1.80 | na |
Getting Started
DRP-AI TVM is a tool that generates runtime executables for AI from trained AI models for Renesas' RZ/V Series MPUs. Below is the overview of the Renesas DRP-AI TVM Tool.

Translate TVM Models
RZ/V2H Rapid Evaluation (Yolo) Wiki
RZ/V2 Evaluation (Yolo) Wiki
TVM Application Development
A summary of the TVM API implementation is DRP-AI TVM Application Development.
The link below shows the performance of several AI Vision Models converted using the TVM and Tested on the RZV2MA. The TVM is capable of converting modesl from exported trained models in the standard ONNX format, pyTorch IMage Models TIMM, and Pytorch Class Models.
Official DRP-AI TVM Performance
DRP-AI TVM Sample Applications
RZ/V Web Performance Application
This Application runs AI Algorithms, translated using the Renesas TVM on the RZ/V products. The image, AI output and performance are viewed on a web client ( i.e. PC browser ). Source code running on the RZ/V and web hosting software can be found in the link above. List of AI Models implemented for the demo can be found here.
RZ/V TVM Application Example
This demo demonstrates how to write an application that implements a DRP-AI TVM generated model. The demo uses Resnet50.
Tested AI Models
These are the models Renesas has tested on the Renesas DRP-AI TVM Tool.
Renesas TVM Models
DRP-AI TVM subgraph profiling ("DRP-AI" or "CPU" processing)
To analyze the subgraph processing of DRP-AI TVM please refer to the profiling guide.
DRP-AI TVM profiling
The ONNX of the subgraphs assigned to DRP-AI are saved in the temp subdirectory after the AI model is compiled.