General Information

  • Software Downloads
    • RZ/V2H Linux Package
    • Mali Graphic Library
    • Video Codec Library
    • ARM Mali Full ISP
    • RZ/V2L DRP-AI Support Package
    • RZ/V2H Cortex-M33 and Cortex-CR8 Multi-OS Package (optional)
    • Robotic Operating System (ROS)
    • RZ/V2H Cortex CM33 FSP

Prebuilt Images

RZ/V2H AI SDK

AI SDK Contents:

eSD Card Image

    • The eSD Card Image is a prebuilt yocto image that contains the following yocto packages
      • VLP Linux
      • ARM Mali Graphics ( limited license )
      • Codec ( limited license )
      • DRP-AI Driver
      • OpenCVA ( DRP Accelerated )
  • Β 
    • The eSD Image DOES NOT include the following
      • e-CON MIPI Camera ( Contact e-CON Systems )
      • AI SDK Demos ( Coming Soon )

TVM Translator Environment

    • The TVM Translator is the recommended translator to translate AI models for the DRP-AI Driver. All the AI SDK demos use the TVM Translator. Included in the AI SDK is the DRP-AI Translator. This translator is needed for TVM installation and does not need to be installed. Installation using Docker is recommended because the TVM Environment requires a PC running Ubuntu 20.04. For information about Docker setup see here.
    • For information about using the TVM Translator see the Official Site here.
    • NOTE: Once the AI SDK Environment is setup the TVM will be installed in the the root directory /drp_tvm_sdk

Available Demos

DRP-AI

  • vSLAM (Contact Sales Representative for demo)
  • DRP-AI Demos
    • Included with the DRP-AI Package. AI models include
      • Classification (Resnet50)
      • Object Detection ( YoloX and Yolov2 )
      • Segmentation ( DeepLabv2 )
  • Renesas RZ/V2H AI SDK
AI SDK Application Repository

The AI SDK repository contains many AI Demos. This repo contains source, pre-compiled application, and Translated AI Models for DRP-AI. This make the repository very large. Below is a method to download single demo

Download R01_object_detection
git clone --depth 1 --filter=blob:none --sparse \
  https://github.com/renesas-rz/rzv_ai_sdk.git
cd test-git-partial-clone-big-small
git sparse-checkout set R01_object_detection


RZ/V2H vSLAM Sample CodeΒ 

  • This is a YOLO-Planar-SLAM-DRP system developed based on YoloPlanarSLAM.
    This SLAM can improve tracking accuracy by removing moving object (human) with object detection AI model (YOLO).
    Renesas' high-performance AI accelerator (DRP-AI) enable to operate YOLO in real-time.
  • By company Computermind
  • https://github.com/ComputermindCorp/yolo-planar-slam-drp

DRP-AI Tools

AI Model to DRP-AI Hardware Translation Flow. For Sparse Model Creation the recommended path after ML Framework is S1, S2, S3. For Dense Model Creation after ML Framework is D1, D2.

AI Model to DRP-AI Hardware Translation Flow. For Sparse Model Creation the recommended path after ML Framework is S1, S2, S3. For Dense Model Creation after ML Framework is D1, D2.

⚠️ The DRP-AI Tools will only work in Ubuntu 20.04

⚠️ the flow S1 is using the pruning CLI tool. The Pruning tool also includes python expansion pack, so S1 can be integrated into the ML Framework training step.

(S1) RZ/V2H Expansion Pack (Pruning Tool )

The DRP-AI MAC supports sparse arrays (unstructured pruning). The expansion pack includes CLI and python libraries (expansion pack). The expansion pack allows for integration of the Pruning process into the ML Frameworks for training. The Expansion Pack supports Pytorch, Tensorflow, and Tensorflow-lite.

Official Site

(S2,3 or D1,2 ) RZ/V2H DRP-AI TVM

TVM Repository

DRP-AI TVM wiki

DRP-AI Application Development

The Renesas TVM is the DRP-AI translator tool that converts standard ML Frameworks ( Pytorch, Tensorflow, ONNX, .. ) to DRP-AI Hardware object files. The TVM for RZ/V2H includes the following tools. This is the recommended tool for AI Model Translation to the DRP-AI.

  • Inference Pre-processing Configuration
  • Quantization Tool
  • Translation Compiler

RZ/V2H DRP-AI Translator and Quantization Tool

Official Site

This tool is used by the TVM for translation of AI Models. It is needed to to install the TVM. ( AI SDK includes this )

For Advance Translation this tool can also be used for AI Model translation instead of the Renesas TVM. Only AI Model operations listed in the RZ\V2H DRP-AI Translator Manual ( section 4.1) can be used with this translator. For AI models that have un-supported operations please use the Renesas DRP-AI TVM Tool. The tool supports quantization and translation of AI Models exported in the ONNX format to the RZ/V2H DRP-AI (INT8) hardware. This tool includes the following

  • RZ/V2H DRP-AI Translator
  • DRP-AI Quantization Tool

The RZV2H DRP-AI MAC only performs INT8 operations, so AI Models must be quantized before translation.

Retraining Quantized Models

It is recommended to retrains a model after quantization to reduce changes to the inference accuracy . For that purpose the Quantization tool includes optional parameters that point to the data set and dataset parsing function.

Beside the AI Model below are additional items needed to properly quantize a model.

  • Customer Dataset ( does not need to be the full dataset )
  • Function to parse the mode

Image Processing

OpenCV

  • By default OpenCV is included AI SDK.
  • OpenCV Version 4.1
  • DRP Acceleration
    • OpenCV DRP Acceleration uses the RZ/V2H DRP ( not DRP-AI ) hardware IP
      • Accelerated OpenCV functions: TBD
    • Released : TBD
    • Uses the DRP ( not DRP-AI ) hardware IP

Getting Started

The RZV2H AI SDK page is the recommended place to start evaluating the RZ/V2H EVK. The page includes detailed information about setup of the EVK, and of the AI SDK Development Environment. Building a Yocto BSP,. links to Yocto Packages and information is here..

RZ/V2H AI Applications Tutorial Getting Started | Renesas

Setup AI SDK Environment and Evaluate Prebuilt Image

Yocto Build

The Renesas AI SDK includes information about building the AI SDK using the Yocto Build Framework. This is recommended to customize the Linux BSP.

The BSP includes the following packages

  • RZ/V2H Linux VLP
  • DRP-AI Drivers
  • DRP OpenCV Accelerator
  • Mali Graphics ( Restricted License )
  • Renesas Codec ( H.265/H.264 ) ( Restricted License )

Not included

  • Demos ( see here for information )
  • e-Con MIPI Driver ( see link )
    • follow step 5 to install e-CON Camera
  • Unrestricted Mali Graphics and Codec License
  • CM33 and CR7 Multi-OS Support and FSP ( Coming Soon )

CM33 and CR7 Multi-OS and FSP

This has not been released for RZ/V2H yet.

Hardware

Power Supply

Recommended Power Supplies ( Recommend 100Ws )


DescriptionLinkComments
πŸ™‚Amazon BasicsLink2xUSB-C, 2xUSB,

1x65-100W, 1x18W, 2x12W

πŸ™‚NekteckLink1x USBC 100W

LCD Monitor

Known working LCD Monitors

ResolutionTouchscreenDescriptionLinkComments
πŸ™‚1920x1080YesWimaxit 14 InchπŸ›’ buyThis is a very nice screen. Good color and easy to press the icons. The LCD input is mini-HDMI and comes with a mini-HDMI to HDMI cable. The RZ board is micro-HDMI. You will also need to buy a HDMI to micro-HDMI adapter. Or, buy a mini-HDMI to HDMI-micro cable. Note the the micro-USB connection on the LCD for touchscreen does not work, but the USB-C connector does work for touchscreen. You will simply need a USB-C to USB-A cable or adapter.
πŸ™‚1920x1080YesELECROW 10.1 InchπŸ›’ buyThis is a very nice screen. You will also need to buy a HDMI to micro-HDMI cable.
πŸ™‚1280x800YesSunFounder 10.1 inchπŸ›’ buyAll the cables that you will need are included.
πŸ™‚1024x600YesIngcool 7 inch
7IP-CAPLCD
πŸ›’ buyIf you attach the 'Touch' USB connection on the LCD to the RZ/G2L board, it will both power the LCD board as well as enable touch support. This kit comes with HDMI cables.
πŸ™‚800x480YesGeeekPi 5 Inch
EP-0081
πŸ›’ buyHDMI cable not included.

MIPI Camera

Supported MIPI Cameras

NOTE: All Camera Drivers ( MIPI and USB 3.2 ) are supplied by the Camera Manufactures.Β Β 

1: Contact e-Con for camera module and driver


ResolutionsDescriptionLinkComments
πŸ™‚VGA ( 640x480) , HD ( 1270x720), FHD(1920,1080)

Format YUYV FPS 30 and 60

e-CAM22_CURZHLinkThis Camera was designed for the EVK MIPI Connector Interface. Uses the Sony Starvis I IMX462.

2MPe-CAM25_CURZHLink12MP/ Global Shutter, ISP,AE0234

8MPe-CAM80_CURZHLink18MP / Rolling Shutter, e-con provides RZ ARM Mali ISP binary, IMX415, Requires RZ ISP support Pkg.

8MPe-CAM85_CURZHLink18MP / Rolling Shutter, e-con provides RZ ARM Mali ISP binary, IMX715, Requires RZ ISP support Pkg.

8MPe-CAM8X_CURZHLink18MP / Rolling Shutter, ISP, AR0830

5MPNileCAM57_CURZHLink15MP / Global Shutter, RGB-IR, ISP, OX05B1S
πŸ™‚1MP - 8MPTEVS-AR0xxxx-xLink

Adapter and modules compatible with the RZ/V2H EVK by TechNexion Embedded Vision Solutions.Β Promotion Video

πŸ™‚8MPV2H IMX415LinkRGB, 8MP / Rolling Shutter. Supports multi camera sync. Requires RZ ISP support Pkg.Β 

Thermal Temperature

This feature is supported in AI SDK 5.0 and later. Enabled by default.

The RZV2H has two thermal zones

  • zone0 - includes MCU Coprocessor CM33 and DRP-AI MAC
  • zone1 - includes MPU Quad Cortex CA55, DRP-AI MAC, ARM Mali GPU, and othersΒ  Β 

RZ thermal usage click here.

  • No labels