RZ/A Series 32/64-bit MPUs This page is for the Renesas RZ/A family of embedded SoCs. The main goal is to make the information about RZ/A SoCs friendly, easy to access for embedded developers.
RZ = Renesas Zenith
Online Resources
The links below can be used to get familiar with Renesas RZ/A SoC
Below are links to Source code for the RZ/A bootloaders and firmware update. These are reference code that was designed for the Renesas RZ/A EVKs. Included below are links to porting documentation.
RZA1
RZ/A1 Bootloader
RZ/A1H Group Example of Booting from Serial Flash MemorydocandSource Code