You are viewing an old version of this page. View the current version.

Compare with Current View Page History

« Previous Version 6 Next »

 RA Series 32-bit MCUs

Introduction

This page is for the Renesas RA family of MCUs. The main goal is to make the information about RA MCUs friendly, easy to access for embedded developers.

The links below can be used to get familiar with Renesas RA MCUs. 

Getting Started with RA

Here are the resources for RA MCUs on Renesas GitHub site.

  • Flexible Software Package (FPS)
  • Example Projects (EPs)
  • Application Project (APs) 

Other resources on Renesas Website.  Links below are pre-configured searches.  You can modify them as needed.  

First RA Project

 Steps below are for creating a simple Blinky project with Renesas supported tools.  e2studio is the Renesas supported IDE. You can also use EWARM and Keil IDEs.  Supported toolchains are Arm GNU Toolchain, LLVM Embedded Toolchain for Arm, IAR Compiler, and Arm Compiler.  

  • Download the latest FSP platform installer from here for e2studio for Windows.  It includes Arm GNU and LLVM toolchains.  








Official Software and Documentation

These are the currently supported Software packages for the RZA1 and RZA2M. The

Renesas Supported Development Environments

  • Renesas e2studio
  • RZA1 Smart Configurator
    • NOTE: The RZA1 is not supported on the Smart Configurator found in the Renesas e2studio IDE.
    • This Smart Conjugator is a standalone application
    • Hardware Pin Configuration is supported
    • Code Generation not supported

RZA GUI Platforms

RZA Bootloaders

Below are links to Source code for the RZ/A bootloaders and firmware update. These are reference code that was designed for the Renesas RZ/A EVKs. Included below are links to porting documentation.

RZA1

  • RZ/A1 Bootloader
    • RZ/A1H Group Example of Booting from Serial Flash Memory doc and Source Code
    • RZ/A1LU QSPI Flash Boot Loader doc and Source Code
    • RZ/A1LU Group Example of Booting from Serial Flash Memory doc and Source Code
  • RZA firmware update
    • The RZA1 does not have Firmware Update reference code.
    • Refer to the RZA2M Firmware Update for Serial Flash Driver to port to the RZA1.

RZA2M

Porting Guides

RZ/A1

  • RZ/A1 Azure Porting Guide gear Wiki

Articles and Whitepapers

Topics

🎥 Demo Videos

FAQ

  • No labels