You are viewing an old version of this page. View the current version.

Compare with Current View Page History

« Previous Version 17 Next »

RZ/A Series 32/64-bit MPUs

Introduction

This page is for the Renesas RZ/A family of embedded SoCs. The main goal is to make the information about RZ/A SoCs friendly, easy to access for embedded developers.

The links below can be used to get familiar with Renesas RZ/A SoC

Boards

  • Here is the list of available Renesas Evaluation Boards (bottom of page).
  • The board pages below contain instructions for downloading and building the BSP as well as other useful information about the boards.

RZ/A3 Series Evaluation Boards


RZ/A2M Series Evaluation Boards


RZ/A1 Series Evaluation Boards


RZ/A1UL GR-LYCHEE

by Renesas MBED

RZ/A1H GR-PEACH

by Renesas MBED



Official Software and Documentation

These are the currently supported Software packages for the RZA1 and RZA2M. The

Renesas Supported Development Environments

  • Renesas e2studio
  • RZA1 Smart Configurator
    • NOTE: The RZA1 is not supported on the Smart Configurator found in the Renesas e2studio IDE.
    • This Smart Conjugator is a standalone application
    • Hardware Pin Configuration is supported
    • Code Generation not supported

RZA GUI Platforms

RZA Bootloaders

Below are links to Source code for the RZ/A bootloaders and firmware update. These are reference code that was designed for the Renesas RZ/A EVKs. Included below are links to porting documentation.

RZA1

  • RZ/A1 Bootloader
    • RZ/A1H Group Example of Booting from Serial Flash Memory doc and Source Code
    • RZ/A1LU QSPI Flash Boot Loader doc and Source Code
    • RZ/A1LU Group Example of Booting from Serial Flash Memory doc and Source Code
  • RZA firmware update
    • The RZA1 does not have Firmware Update reference code.
    • Refer to the RZA2M Firmware Update for Serial Flash Driver to port to the RZA1.

RZA2M

Articles and Whitepapers

Topics

FAQ

  • No labels